This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 Read/Write Time



Hello,

I just write and read 10 MByte to/from DDR3 memory as below.

Write:

for(i=0;i<(10*1024*1024);i=i+4)
{

    *(volatile uint32_t *)(DDR3_START_ADDR + i) = data;

}

Read:

for(i=0;i<(10*1024*1024);i=i+4)
{
       data = *(volatile uint32_t *)(DDR3_START_ADDR + i);
}

When I compared, the write and read data were same, but the wring/reading time took quit longer than I expected.

Writing 10MB took about 80ms, reading took about 257ms at 1.25GHz core clock is 1.25GHz and 667MHz DDR3 clock.

Questions are

1> Is it normal that reading time takes longer time than writing?

2> The time I measured reasonable?

3> How to improve reading/writing time.