This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Aaron,
Please give the full version number in the form of 01.00.xx.yy. This can be found in the Release Notes.
Regards,
Mohammed Harris
Hi, Harris
Thanks for your reply, the version number is : 01.00.09.00
thank you very much again :)
Hi, Harris
Thanks for your reply, the version number is : 01.00.09.00
thank you very much again :)
Mohd. Harris said:Aaron,
Please give the full version number in the form of 01.00.xx.yy. This can be found in the Release Notes.
Regards,
Mohammed Harris
Hi,
We are able to change dynamically quality factor and resolution from release version 500.V.MJPEG.E.IVAHD.01.00.09.00 and encoded images are also proper.
dynamicParams.videnc2DynamicParams.inputHeight = 640;
dynamicParams.videnc2DynamicParams.inputWidth = 480;
dynamicParams.qualityFactor = 75;
retValue = JPEGVENC_control(handle, XDM_SETPARAMS,
(JPEGVENC_DynamicParams *)&dynamicParams,
(JPEGVENC_Status *)&status );
Can you try to initialize dynamic params and then call Control Call with XDM_SETPARAMS for dyanmic change of params.
The values that you get by calling XDM_SETPARAMS are the actual values used by the encoder. Could you check if these values match with those that you set through dynamic params.