This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can a 8-bit input ports like VIN0[A] of DM8168 capture 1080p@30?

HI!

Our company wants to use DM8168 to capture 4-ch 1080p@30 from HD-SDI camera.

The stream  from sdi deserializer is a 10-bit   inteleave Y/C  data.

Can a 8-bit input ports like VIN0[A] of DM8168 capture 1080p@30? The pixel clock is 148.5MHZ

Can a 8-bit input ports directly capture the 10-bit   inteleave Y/C  data? Is need a FPGA?

I have seen some information  from  High-Definition Video Processing Subsystem Technical Reference Manual

• 8-bit input ports:
– A single non-multiplexed CIF/480i/480p/720p/1080i Y/C data
– Up to 2-stream multiplexed ED (480p) Y/C data
– Up to 4-stream multiplexed SD (480i) Y/C data
– Up to 8-stream multiplexed CIF Y/C data
• 16/24-bit input ports:
– A single non-multiplexed CIF/480i/480p/720p/1080i/1080p Y/C data
– A single 24-bit YCbCr component or raw RGB data
– Up to 2-stream multiplexed HD (720p/1080I) Y/C data
– Up to 4-stream multiplexed ED (480p) Y/C data
– Up to 8-stream multiplexed SD (480i) Y/C data
– Up to 8-stream multiplexed CIF Y/C data

I want to have a precise answer.

thanks!