Other Parts Discussed in Thread: DM385
Hi All,
We have a DM385 based custom board, we use camera sensor on I2C[3] using IPNC RDK 3.5.
Following are the pinmux and clock details.
After bootup value of CM_ALWON_I2C_1_CLKCTRL (0x48181568) is 0x00000002.
i2c3 mux0 PINCNTL22/23 are used value of 0x4814 0854 & 0x4814 0858 are 0x000E0020.
With this above changes we could able to do read/write from u-boot, but from M3VPSS firmware its hangs after calling the function "Iss_device16AddWrite8" and i2c3_scl line pulled low.
[m3video] 3306: SYSTEM : System Video Init in progress !!!
[m3vpss ] 3306: SYSTEM : System VPSS Init in progress !!!
[m3video] 3306: SYSTEM : System Video Init Done !!!
[m3vpss ] 3306: SYSTEM: All VPDMA Free !!!
[m3video] 3307: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_0] in region 0 ...
[m3vpss ] IN Vps_platformTI8107SetPinMux
[m3video] 3307: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_0] in region 0 ...
[m3video] 3307: SYSTEM: ListElem Shared Addr = 0xbe984180
[m3video] 3310: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_1] in region 0 ...
[m3video] 3310: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_1] in region 0 ...
[m3video] 3310: SYSTEM: ListElem Shared Addr = 0xbe987680
[m3video] 3322: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_28] in region 0 ...
[m3vpss ] === I2C0/2 Clk is active ===
[m3video] 3322: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_28] in region 0 ...
[m3vpss ] === I2C1/3 Interface Clk is active ===
[m3video] 3322: SYSTEM: ListElem Shared Addr = 0xbe98ab80
[m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to VPS_PLATFORM_CPU_REV_1_0
[m3video] 3325: SYSTEM: Creating ListMP [VIDEO-M3_IPC_OUT_29] in region 0 ...
[m3vpss ] IN Iss_platformTI814xSetPinMux
[m3video] 3325: SYSTEM: Creating ListMP [VIDEO-M3_IPC_IN_29] in region 0 ...
[m3vpss ] PLATFORM: UNKNOWN CPU detected, defaulting to ISS_PLATFORM_CPU_REV_2_1
[m3video] 3325: SYSTEM: ListElem Shared Addr = 0xbe9a4800
[m3vpss ] 3325: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_0] in region 0 ...
[m3vpss ] 3326: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_0] in region 0 ...
[m3vpss ] 3326: SYSTEM: ListElem Shared Addr = 0xbe9be480
[m3video] 3327: HDVICP: Doing PRCM for IVAHD[0] ...
[m3vpss ] 3329: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_1] in region 0 ...
[m3video] 3328: HDVICP: PRCM for IVAHD[0] ... DONE.
[m3vpss ] 3329: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_1] in region 0 ...
[m3video] 3328: SYSTEM : Initializing Links !!!
[m3vpss ] 3329: SYSTEM: ListElem Shared Addr = 0xbe9c1980
[m3video] 3329: SYSTEM : FREE SPACE : System Heap = 2089032 B, Mbx = 10240 msgs)
[m3vpss ] 3345: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_23] in region 0 ...
[m3vpss ] 3345: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_23] in region 0 ...
[m3video] 3329: SYSTEM : FREE SPACE : SR0 Heap = 15985024 B (15 MB)
[m3vpss ] 3345: SYSTEM: ListElem Shared Addr = 0xbe9c4e80
[m3video] 3329: SYSTEM : FREE SPACE : Frame Buffer = 110100352 B (104 MB)
[m3vpss ] 3348: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_24] in region 0 ...
[m3vpss ] 3348: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_24] in region 0 ...
[m3video] 3329: SYSTEM : FREE SPACE : Bitstream Buffer = 78643072 B (74 MB)
[m3vpss ] 3349: SYSTEM: ListElem Shared Addr = 0xbe9e4880
[m3vpss ] 3352: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_25] in region 0 ...
[m3video] 3329: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
[m3vpss ] 3352: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_25] in region 0 ...
[m3video] 3330: SYSTEM : FREE SPACE : Tiler Buffer = 127 B (0 MB) - TILER OFF
[m3vpss ] 3352: SYSTEM: ListElem Shared Addr = 0xbea04280
[m3vpss ] 3359: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_28] in region 0 ...
[m3vpss ] 3360: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_28] in region 0 ...
[m3vpss ] 3360: SYSTEM: ListElem Shared Addr = 0xbea23c80
[m3vpss ] 3363: SYSTEM: Creating ListMP [VPSS-M3_IPC_OUT_29] in region 0 ...
[m3vpss ] 3363: SYSTEM: Creating ListMP [VPSS-M3_IPC_IN_29] in region 0 ...
[m3vpss ] 3363: SYSTEM: ListElem Shared Addr = 0xbea3d900
[m3vpss ] 3365: SYSTEM : HDVPSS Drivers Version: HDVPSS_01_00_01_37
[m3vpss ] 3366: SYSTEM : FVID2 Init in progress !!!
[m3video] 3387: SYSTEM : Initializing Links ... DONE !!!
[m3vpss ] 3430: SYSTEM : FVID2 Init in progress DONE !!!
[m3vpss ] 3431: SYSTEM : Device Init in progress !!!
[m3vpss ] Iss_init called !!!!!!
[m3vpss ] Iss_csi2 init called !!!!!!
[m3vpss ] CPIS_init DONE !!!!!!
[m3vpss ] initPrms.isI2cInitReq = 1
[m3vpss ] initPrms.isI2cInitReq = 1
[m3vpss ] PSP_i2cInit 0
[m3vpss ] PSP_i2cInit 1
[m3vpss ] PSP_i2cInit 2
[m3vpss ] PSP_i2cInit 3
[m3vpss ] Vps_deviceInit Daughter card not detected/connected!
[m3vpss ]
[m3vpss ] TI_8107_BUILD
[m3vpss ] 3617: SYSTEM : Device Init in progress DONE !!!
[m3vpss ] gOv5640_I2c_ctrl.i2cInstId is 3
[m3vpss ] Iss_device16AddWrite8
Please help me to solve this.
Regards,
Manoj