Hi,
We have develop DM388 base IPNC.
DM388 provides internal watchdog time.
I had enabled watchdog in kernel. Application is opening watchdog driver and send keep alive periodically.
If Application kills or hang watchdog resets CPU.
We also uses AJ30 pin (RSTOUT_WDT_OUT) pin to provide reset signal to all peripheral ics in case to reboot via watchdog.
At power on reset time RSTOUT_WDT_OUT pin is low and then become high after processor come out of reset. We had connected external pull up.(10K)
Problem: If watchdog timer reaches zero and processor reboots this RSTOUT_WDT_OUT pin is not provide any signal and remains high only.
Please provide solution on this.
Regards,
Kunjal