This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

initramfs kernel compile error



Hi, everyone 

I follow the doc initrd.pdf to compile kernel include initramfs, my step:

1 cd to the directory of my target file system and execute command : find . | cpio -H newc -o > ../target_fs.cpio

2 I use menuconfig to config the kernel , some of the detail of .config file is like this: 

....

CONFIG_BLK_DEV_INITRD = y

CONFIG_INITRAMFS_SOURCE="/usr/local/ezsdk/filesystem/arago-base-tisdk-image-dm814x-evm.cpio"

............

CONFIG_BLK_DEV_RAM = y

CONFIG_BLK_DEV_RAM_COUNT = 1

CONFIG_BLK_DEV_RAM_SIZE = 81920

.....

3 and then I execute the make command to compile the kernel. 

at the end of the compilation, the log prompt:

arch/arm/kernel/head.o: in function "__enable_mmu_end":

(.head.text+0x304):relocation truncated to fit:R_ARM_JUMP24 against ‘__fixup_a_pv_table'

make: *** [.tmp_vmlinux] error 1

is there anything else I have to do to?

another question when I read initrd.pdf 

what is the meaning of "Note: To be able to detect initramfs by kernel properly, the top level directory has to contain a program called init.For example, this can be done by using a soft link from top level init to /bin/busybox (assuming you are using BusyBox in your initramfs). 

/init -> /bin/busybox

"?Initrd.pdf