This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5x DSPBIOS : tconf: can't create session manager: create of JVM failed

Other Parts Discussed in Thread: CODECOMPOSER

Team,

Forking Kazem's thread on this topic.  I encountered this error on a fresh install of CCS  Version: 6.1.0.00104 using  DSP BIOS bios_5_42_01_09 while building the C5535 Audio Framework (c55_caf_02.00.02.04).

The Error message reads as following and is related to a missing Java something or other.

C:\ti\bios_5_42_01_09\xdctools\C:/ti/bios_5_42_01_09/xdctools/tconf: can't create session manager: create of JVM failed


My verbose build logs can be found on Kazem's thread. 

http://e2e.ti.com/support/embedded/tirtos/f/355/p/411654/1461208

Per the set up instruction the following System Variable was created.

BIOS_INSTALL_DIR --> C:\ti\bios_5_42_01_09

And the xdctool directory (C:\ti\bios_5_42_01_09\xdctools) was appended to the System PATH variable.

Additional behavior of this bug is the following.

Code Composer is unable to open the .TCF configuration file. 

And Windows 7 64bit is unable to run the tconf.exe in the xdctools directory.

I believe this to be the root of the problem and will update this thread once it is resolved.