This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[K2H] Hyperlink/sRIO communication between K2Hs

Hello,

My customer starts to evaluate K2H EVM and is wondering if Hyperlink can be used between two K2H EVM (A15 side, not DSP).
I think the answer is 'yes' when using OpenMPI + RTM-BOC, but my customer does not like to use OpenMPI...
So now my question is ... do you have generic hyperlink linux drivers in kernel, which you could support via e2e ?
If yes, do you have any example application code for that ?

Also, this is just for my understanding, but please let me know about sRIO use case, instead of hyperlink. 
Do you have generic sRIO linux driver in kernel, which you could support via e2e ?
If yes, do you have any example application code for that ?

Best Regards,
Kawada