This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 DDR configuration



Hi all.

I have a question about DDR configuration in DM8148 ARM+DSP custom board. The DDR chip is 2Gb MT41J128M16 – 16 Meg x 16 x 8 banks.
I cannot quite understand what is the correct DMM_LISA..0-3 registers configuration. Why are there 4 registers and the first 2 are not used?
How should i configure this registers according to the layout i have?
my current configuration is:

PG2_1_DMM_LISA_MAP__0    0x0
PG2_1_DMM_LISA_MAP__1    0x0
PG2_1_DMM_LISA_MAP__2    0x80540300
PG2_1_DMM_LISA_MAP__3    0xC0540300

DDR3_EMIF_REF_CTRL            0x00000C30
DDR3_EMIF_SDRAM_CONFIG 0x61C01032
DDR3_EMIF_SDRAM_ZQCR     0x50074BE1

My bootargs are:

console=ttyO3,115200n8 no_console_suspend rootdelay=2 rootwait noinitrd earlyprintk print_fatal_signals=1 nolock irqpoll boot_delay=5 rw root=/dev/mmcblk0p6 vram=50M ti814xfb.vram=0:24M,1:16M,2:6M notifyk.vpssm3_sva=0xbf900000 mem=248M ddr_mem=1024M debug=1 5

I also use firmware_loader with the dm8148_hdvpss.xem3 default memory map file to load VPSS core.

I get these weird alignment exceptions and memory faults sometimes during firmaware_loader VPSS firmware loading and sometimes during kernel loading and rarely when loading DSP core. Which leads me to think it's some sort of memory problem/misconfiguration. 
I couldn't find anywhere a good manual that explains how to get the correct configuration for the DDR registers for dm8148. 

Can someone tell me what's the correct LISA_MAP__* and EMIF_SDRAM_*  registers for my chip, or even better, where i can learn how to retrieve that information myself :D 

Much Appreciated.


Boris-Ben Shapiro