Hello all,
I have modified project "Hello world" from
mcsdk_2_01_02_06\tools\boot_loader\examples\pcie\
to run this example on Core0 and Core1 in the L2SRAM
with the same codes for both cores.
To copy codes from Core0 to Core1 I used memcpy function.
All worked properly except one problem:
after operation
*(volatile uint32_t *)(IPCGR(1))=(1)
all valuable content of DDR (that was previously filled from Linux-host program)
was zeroized.
Please answer two question:
- why IPCGR zeroizes DDR;
- how to save the content of DDR during IPCGR.
I used:
Code Composer Studio 5.2.1.00018
mcsdk_2_01_02_06
MDSEVM6678L/MDXEVMPCI board
Best regards,
Stanislaw