Other Parts Discussed in Thread: AM4372
Hi,
I have questions about AM437x Linux SDK.
My customer are using "ti-processor-adk-linux-am437x-evm-01.00.00.00" and
they modified AM437x-GP-EVM base DTS(Device Tree Source) for their custom board.
But following error occured and having kernel panic:
"
[ 0.207377] omap_l3_noc 44000000.ocp: L3 debug error: target 8 mod:0 (unclearable)
[ 0.207406] omap_l3_noc 44000000.ocp: L3 debug error: target 13 mod:1 (unclearable)
[ 0.207454] omap_l3_noc 44000000.ocp: L3 application error: target 8 mod:0 (unclearable)
[ 0.207473] ------------[ cut here ]------------
[ 0.207506] WARNING: CPU: 0 PID: 1 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x234/0x35c()
[ 0.207519] 44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET L4_WKUP (Read): Data Access in User mode during Functional access
"
Q1. What does following message mean and what kind of case does this error occur?
"44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET L4_WKUP (Read): Data Access in User mode during Functional access"
best regards,
g.f.