Hi,
Refer to the 6657 EVM board has developed a 6657 board.
JTAG hardware circuit is as follows
Test Connection is ok
but 90% could not work properly (Sometimes this is successful)
no bootmode
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Senthil,
Thank you for the quick reply,
C6657 EVM DDR3 MEMORY INTERFACE (MT41J128M16HA-125)
my custom board DDR3 MEMORY INTERFACE (MT41K256M16HA-125)
I only changed here,
I want to know where there is need to be aware of, and where need to modify?
And why sometimes success sometimes not successful?Be a hardware problem?