Hi,
Regarding the ISDK Example EtherNet/IP provided in latest ISDK(02.01.00.01),
the user guide(wiki) mentions,
"This example is a limited demo application that is constrained so that a user will be
allowed to execute it for one hour only"
Does it mean we cannot run this demo more than 1 hour? please let me know the details of this restriction.
Meanwhile we would like to use this EtherNet/IP sample application to test a
standard TCP/IP ethernet application on AM437x IDK.
We successfully tested standard TCP/IP before with AM335x IDK + older ISDK version with the
help of below E2E guidance.
e2e.ti.com/.../318653
We would like to know if we can do the same test(standard TCP/IP) on AM437x IDK board?
like commenting out the EIP specific calls (like GetAssignedIP(); EIPMain();)..
Best Regards
Kummi