This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Keystone2 Linux: UDP packet loss

Expert 1800 points

Other Parts Discussed in Thread: 66AK2H06

Hello,

We are having custom board based on 66AK2H06.  We are losing  UDP packets between two custom boards.  Port 0 is interfaced to FPGA which in turn is connected to backplane. The two custom boards talk to each other over backplane.  One of the application from board 1 sends bursty traffic less than 50Mbps.  We see that the packets are lost.  There are no RcvBuf errors and InErrors reported in linux kernel.  

No errors seen in CPSW statistics as seen by following command.

ethtool -S eth0

There are no drops seen in any of the socket Qs when observed using

cat /proc/net/udp.

We have a FPGA probe which monitors the sequence number of the packets for all the ports.  When the packet loss happens, we do not see any packet lost until the FPGA nor in Linux.  The packets are dropped somewhere between FPGA and CPU.  Is that possible to get additional debug information on the switch statistics.

Is there any additional configuration required for CPSW ?

Please clarify

Thanks

Rams

  • Hi
    We are trying to send UDP traffic using iperf and the FPGA in Board 2 (Receiver Board) is probing the incoming UDP traffic on port 5001. The FPGA probe counter sees all the packets at the receiving end. But the packets are lost at CPU and not seen in Linux.
    Please see below the log from iperf, netstat and FPGA probe.

    ~ $ iperf3 -c 192.168.0.104 -u -b 200M -l 1500 -p 5001
    Connecting to host 192.168.0.104, port 5001
    [ 4] local 192.168.0.102 port 58203 connected to 192.168.0.104 port 5001
    [ ID] Interval Transfer Bandwidth Total Datagrams
    [ 4] 0.00-1.00 sec 21.5 MBytes 181 Mbits/sec 15063
    [ 4] 1.00-2.00 sec 24.9 MBytes 209 Mbits/sec 17426
    [ 4] 2.00-3.00 sec 22.7 MBytes 191 Mbits/sec 15899
    [ 4] 3.00-4.00 sec 25.4 MBytes 213 Mbits/sec 17760
    [ 4] 4.00-5.00 sec 22.9 MBytes 192 Mbits/sec 16039
    [ 4] 5.00-6.00 sec 25.3 MBytes 212 Mbits/sec 17656
    [ 4] 6.00-7.00 sec 22.5 MBytes 189 Mbits/sec 15748
    [ 4] 7.00-8.00 sec 23.9 MBytes 201 Mbits/sec 16739
    [ 4] 8.00-9.00 sec 23.4 MBytes 197 Mbits/sec 16380
    [ 4] 9.00-10.00 sec 23.5 MBytes 197 Mbits/sec 16435
    - - - - - - - - - - - - - - - - - - - - - - - - -
    [ ID] Interval Transfer Bandwidth Jitter Lost/Total Datagrams
    [ 4] 0.00-10.00 sec 236 MBytes 198 Mbits/sec 0.022 ms 4096/165145 (2.5%)
    [ 4] Sent 165145 datagrams

    iperf Done.


    ################## Board 1 Receiver: ###############################

    ~ $ netstat.arm -s
    Ip:
    1421153 total packets received
    0 forwarded
    0 incoming packets discarded
    1097051 incoming packets delivered
    590165 requests sent out
    173 fragments dropped after timeout
    647641 reassemblies required
    323539 packets reassembled ok
    563 packet reassembles failed
    Icmp:
    67 ICMP messages received
    0 input ICMP message failed.
    InCsumErrors: 0
    ICMP input histogram:
    destination unreachable: 67
    416 ICMP messages sent
    0 ICMP messages failed
    ICMP output histogram:
    destination unreachable: 397
    time exceeded: 19
    IcmpMsg:
    InType3: 67
    OutType3: 397
    OutType11: 19
    Tcp:
    5 active connections openings
    6 passive connection openings
    1 failed connection attempts
    3 connection resets received
    6 connections established
    17357 segments received
    20548 segments send out
    0 segments retransmited
    0 bad segments received.
    1 resets sent
    InCsumErrors: 0
    Udp:
    1053123 packets received
    103635 packets to unknown port received.
    0 packet receive errors
    569302 packets sent
    RcvbufErrors: 0
    SndbufErrors: 0
    InCsumErrors: 0
    UdpLite:
    InDatagrams: 0
    NoPorts: 0
    InErrors: 0
    OutDatagrams: 0
    RcvbufErrors: 0
    SndbufErrors: 0
    InCsumErrors: 0
    error parsing /proc/net/snmp: Success


    ################# FPGA status ####################

    Status 32769: "Packet loss monitor"
    * Timestamp : 2015-09-10 14:01:46.614067
    Packet cnt. : 165146
  • Hi Rams,
    I have seen your post in keystone forum too.
    We can follow it up there.

    e2e.ti.com/.../451659
  • Hi Rams,

    As of now, closing this post here as it already exist here. e2e.ti.com/.../451659

    -----