This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Just bought this kit for evaluation. I'm trying to use hardware acceleration for ssl (AES128-SHA cipher).
I've seen that there was an issue with SHA acceleration, was it fixed?
I'm using ti-sdk-am335x-evm-06.00.00
I've created self signed certificate and run on board
openssl s_server -accept 4000 -cert ./root.crt -key ./root.key
if I run openssl s_client -connect 192.168.10.87:4000 -cipher AES128-SHA from the same board it works as expected.
but if I run openssl s_client -connect 192.168.10.87:4000 -cipher AES128-SHA from pc linux computer then I get
ACCEPT
ERROR
1074476768:error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac:s3_pkt.c:479:
shutting down SSL
CONNECTION CLOSED
ACCEPT
Thank you for your help.
Hi,
Thank you very much for help.
I've downloaded ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install and am335x-evm-01.00.00.03.img.zip.
It's a little bit strange to see newer version with number (1) less than older one (6).
Now basic openssl works as expected. So I would assume that hardware acceleration is working.
I see performance degradation when I'm enabling HW acceleration. Is it normal? I would expect HW be faster on large block (I'm usually around 1k).
I will continue to check but as an example my app shows throughput around 3-5mbps with HW (and after awhile it gets lower to the point when my clients starts to disconnect because of timeouts) and around 7mbps without it.
Regards,
Dmitry Efremov.
Dmitry Efremov said:I see performance degradation when I'm enabling HW acceleration. Is it normal? I would expect HW be faster on large block (I'm usually around 1k).
For 1KB data block, the hw crypto should be much faster than sw crypto.
Dmitry Efremov said:I will continue to check but as an example my app shows throughput around 3-5mbps with HW (and after awhile it gets lower to the point when my clients starts to disconnect because of timeouts) and around 7mbps without it.
Do you mind to explain more about your application? How does it use kernel crypto? 3-5 or even 7 mbps is quite low.
Hi,
I've continue to test and it's still not working.
Here is my test case:
ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install and am335x-evm-01.00.00.03.img.zip.
output from server session:
root@am335x-evm:/apollo# openssl s_server -accept 4000 -cert ./root.crt -key ./root.key Using default temp DH parameters ACCEPT -----BEGIN SSL SESSION PARAMETERS----- MFUCAQECAgMDBAIALwQABDATn0ouqFhWn5Eno8DxlfjE4hHK6W9kMjJiXZvb1K/d NrBw1smSsSG8o0ETwVMeYjKhBgIEVZrwkaIEAgIBLKQGBAQBAAAA -----END SSL SESSION PARAMETERS----- Shared ciphers:AES128-SHA CIPHER is AES128-SHA Secure Renegotiation IS supported ERROR 3067688672:error:1408F119:SSL routines:SSL3_GET_RECORD:decryption failed or bad record mac:s3_pkt.c:507: shutting down SSL CONNECTION CLOSED ACCEPT
output from client session
root@am335x-evm:/apollo# cat ./testfile | openssl s_client -cipher AES128-SHA -host localhost -port 4000
CONNECTED(00000004)
depth=0 C = US, ST = CA, L = Some Location, O = Some Company, OU = Some OU, CN = Root, emailAddress = some@email.com
verify error:num=18:self signed certificate
verify return:1
depth=0 C = US, ST = CA, L = Some Location, O = Some Company, OU = Some OU, CN = Root, emailAddress = some@email.com
verify error:num=9:certificate is not yet valid
notBefore=Aug 19 17:40:09 2015 GMT
verify return:1
depth=0 C = US, ST = CA, L = Some Location, O = Some Company, OU = Some OU, CN = Root, emailAddress = some@email.com
notBefore=Aug 19 17:40:09 2015 GMT
verify return:1
---
Certificate chain
0 s:/C=US/ST=CA/L=Some Location/O=Some Company/OU=Some OU/CN=Root/emailAddress=some@email.com
i:/C=US/ST=CA/L=Some Location/O=Some Company/OU=Some OU/CN=Root/emailAddress=some@email.com
---
Server certificate
-----BEGIN CERTIFICATE-----
MIIDkDCCAngCCQDmwYtMXKQOGTANBgkqhkiG9w0BAQsFADCBiTELMAkGA1UEBhMC
VVMxCzAJBgNVBAgMAkNBMRYwFAYDVQQHDA1Tb21lIExvY2F0aW9uMRUwEwYDVQQK
DAxTb21lIENvbXBhbnkxEDAOBgNVBAsMB1NvbWUgT1UxDTALBgNVBAMMBFJvb3Qx
HTAbBgkqhkiG9w0BCQEWDnNvbWVAZW1haWwuY29tMB4XDTE1MDgxOTE3NDAwOVoX
DTI1MDgxNjE3NDAwOVowgYkxCzAJBgNVBAYTAlVTMQswCQYDVQQIDAJDQTEWMBQG
A1UEBwwNU29tZSBMb2NhdGlvbjEVMBMGA1UECgwMU29tZSBDb21wYW55MRAwDgYD
VQQLDAdTb21lIE9VMQ0wCwYDVQQDDARSb290MR0wGwYJKoZIhvcNAQkBFg5zb21l
QGVtYWlsLmNvbTCCASIwDQYJKoZIhvcNAQEBBQADggEPADCCAQoCggEBAMqtbe/v
KtHXRG3+BUlCjzQR7xjWTDNs5PjUJhJ1S2p4cxX1PsWoDTmkcs4uixcMouBMSIon
CFXqA8bVHuqayJumvJgnXaOfNS1bHIXFufO38JNP9JhOsm/lEM4thcOV6Es9T2QH
h302DuE/g7AiV1zkj9mFHd+nG7GnfrIkfNq6Qtp4hwUqVijWq/l3qlepGjEeia9G
1FDeBlp2kW2zEb+rcJMrrgOXzrx+gnG1xObNLTivnHV+M59eCIg3J76cShWtxoaP
e93nzxF9zC3GZemE0SMQY7tOW1aNlKwC1B3w7Huulp1PS/LwWXdxAa+5PJWE6LOU
NNIwlZTUglNKMQkCAwEAATANBgkqhkiG9w0BAQsFAAOCAQEAyYa2FvTYo4gem/pA
sHASjcmhucBYyzANjCn77jGNp8XZisVo816YJ6KK360r0o70V31hsPinU0J8F65A
XzkxIkQDYFK6jlcAIYNX1+rH9/+hohZh329WWT63Uq8rBfZCcDMZBittJZN/SsO7
SM0XSySy16zjjYdyhOu4O/C22nkGKyRpQ40oNG4GivLUC/0wV2h1I3/mF4A9blk8
E1uEisl2tnD0S2yJE5eSHW6Z82a3tAsFJRXgmfOVDARccsP6h0FPM6pWz1VWcecF
cPu8iysrI4CpiRJIEP1YpaSqUIWflPneFMbewm0hlAbkfQkErxo71BeU/25zWhqQ
bzC3HQ==
-----END CERTIFICATE-----
subject=/C=US/ST=CA/L=Some Location/O=Some Company/OU=Some OU/CN=Root/emailAddress=some@email.com
issuer=/C=US/ST=CA/L=Some Location/O=Some Company/OU=Some OU/CN=Root/emailAddress=some@email.com
---
No client certificate CA names sent
---
SSL handshake has read 1253 bytes and written 441 bytes
---
New, TLSv1/SSLv3, Cipher is AES128-SHA
Server public key is 2048 bit
Secure Renegotiation IS supported
Compression: NONE
Expansion: NONE
SSL-Session:
Protocol : TLSv1.2
Cipher : AES128-SHA
Session-ID: C37445DA6F8E77CB4E63D83E35C8BC49CF8623B8A962C5CD8622D90E95FB232C
Session-ID-ctx:
Master-Key: 139F4A2EA858569F9127A3C0F195F8C4E211CAE96F643232625D9BDBD4AFDD36B070D6C992B121BCA34113C1531E6232
Key-Arg : None
PSK identity: None
PSK identity hint: None
SRP username: None
TLS session ticket lifetime hint: 300 (seconds)
TLS session ticket:
0000 - 2f 4f 7d b7 06 45 b1 d2-81 35 11 08 b5 56 78 3f /O}..E...5...Vx?
0010 - 0a 18 94 6f 73 2c e0 02-3e 53 a7 89 e0 9d 40 6e ...os,..>S....@n
0020 - 24 a7 76 3a 80 d6 95 84-9e f1 80 4b 85 dc fb 9a $.v:.......K....
0030 - b1 d0 bf 5a 45 2a f3 f3-47 be e0 bf f8 6c 3e a6 ...ZE*..G....l>.
0040 - 42 12 70 c3 90 39 e8 0f-1d d8 3e c2 8b a3 82 e9 B.p..9....>.....
0050 - de a4 8d 3d d0 8d 7c 80-8f f9 f9 e6 bf 3d 3d cc ...=..|......==.
0060 - 79 3c 15 1b 1a 85 54 bd-21 16 5c ff 8f ab 77 c4 y<....T.!.\...w.
0070 - d2 8e c5 5b 2a 18 9f ca-42 ff 9f 53 82 dd 3b ee ...[*...B..S..;.
0080 - bc ac c6 15 5b ac f9 4c-2d 23 5f 44 83 23 20 5d ....[..L-#_D.# ]
0090 - bb 43 85 fc 00 c3 ff b3-3c 00 ad 9e 17 9f 7c 3d .C......<.....|=
Start Time: 1436217489
Timeout : 300 (sec)
Verify return code: 9 (certificate is not yet valid)
---
3067729632:error:140943FC:SSL routines:SSL3_READ_BYTES:sslv3 alert bad record mac:s3_pkt.c:1289:SSL alert number 20
Hi,
Has anyone tried to repeat it?
I can't continue to evaluate the board because of issue I'm experiencing.