Hello everyone
I want to configure LSU in SRIO by using EDMA. What I want to do is after EDMA receiving a SRIO interrupt event, EDMA would write LSU registers, and then initiate the SRIO transfer. I learn this method from this thread. However, in the section of 7.9.4 EDMA3 Channel Synchronization Events of the C6678 User Manul SPRS691E, I cannot find the SRIO Interrupt.
So can you tell me whether C6678 supports this EDMA configured SRIO operation? If so, which interrupt event is the one triggered by SRIO?
Thanks.
Xining Yu