This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driving Drv8823 : interface with Dm8127

Other Parts Discussed in Thread: DRV8823

Hi,

i want to drive my stepper motor with Drv8823 driver chip, which is directly connected to my Dm8127 board via spi interface.

i've built-in support of spi generic driver module in kernel.

and i applied changes in board specific file with spi_board_info structure..
        {
                .modalias       = "drv8823",
                .irq            = -1,
                .max_speed_hz   = 100000,
                .bus_num        = 1,
                .chip_select    = 1,
                .mode = SPI_MODE_3,
        },
after  spi_register_board_info call i can see spi1.1 file in sys/bus/spi/devices.

i've created node in /dev by mknod -m 666 /dev/spidev1.1 c 153 3.

when i use spidev_test file to send data to driver chip...

i got , "can't open device: No such device or address
Aborted".

what's wrong with this. i guess there is platform specific data is missing.

i don't know how to register platform specific data for this chip,

is there any Linux driver available for drv8823?

regards,

Akash Gajjar