Other Parts Discussed in Thread: AM5728
Hi TI,
We are using AM5728 processor, I could able to fine the links like "processors.wiki.ti.com/.../Sitara_Linux_SDK_Training"
which are explaining about the other processor like am335x etc but not specific to the AM5728 processor and "ti-processor-sdk-linux-am57xx-evm-02.00.00.00" SDK.
ti-processor-sdk-linux-am57xx-evm-02.00.00.00 is based on Linux 4.1.6.x version of Linux and u-boot and the link was reflecting to the older version of Linux and u-boot.
Please refer to the links which are specific to the ti-processor-sdk-linux-am57xx-evm-02.00.00.00 SDK. Documents which are present in SDK are very few. As the Linux in ti-processor-sdk-linux-am57xx-evm-02.00.00.00 is 4.1.6 version I am facing difficulty in browsing the code.
Thanks,
Sudheer.