Using CCS V6.1.1.00022
For AM437x Target
Want to change #define in UART_drv_log.h to CIO_DRV_CONSOLE
This should redirect logging to printf so that we can capture IO using System Analyser.
So we need to rebuild the provided UART library component ti.drv.uart.am437x.aa9fg
There are various Make files within the directory structure which contain references to the correct source files
Have tried invoking from command line using gmake but get "nothing to be done for <etctetc>"
tried deleting the library -- nothing doing
tried editing source to change dates to force rebuild -- nothing doing
created various flavours of project in CCS to suck in the UART library hierarchy and attempted to build -- Loads of build errors with paths and undefined litterals from header files that weren't getting picked up.
Can't find any detailed docs on the best approach to this
Help !!
Si.