Other Parts Discussed in Thread: OMAP3530
Hello Omap experts,
I'm working on an EVM board with an OMAP3530. I have no OS, only stand alone code.
I'm trying to establish communication between OMAP and the embedded power IC through I2C_1 interface.
With my software I'm able to exchange data but I have noticed that the I2C_SCL is not at the expected frequency. In HS mode the SCL is @2.6MHz instead of 3.4MHz.
I have used the following parameters: I2C_SCLL.hsscll = 7 & I2C_SCLL.hssclh = 9.
With observability I've also checked that CORE_96M8FCLK is @96MHz.
I have similar problem in FS mode but it is more obvious in HS.
Any idea of a parameter that I wouldn't have set properly??
Thanks in advance,
Regards.
Nicolas.