This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 SPI Boot parameter (nysh.spi.map)

Genius 5785 points


Hello,

I'd like to understand the "nysh.spi.map" for SPI boot. I saw the following discussion.
e2e.ti.com/.../394292

I also saw "hwPllSetPll" function.
BootROM_c6678_PG2.0\hw\pll\pll.c

It looks like these parameters are strange. I think CPU clock speed is less than 400MHz.

 sw_pll_prediv = 5
 sw_pll_mult = 32
 sw_pll_postdiv = 2
 sw_pll_flags = 1

ex)
- C6670EVM: 122.88MHz * 32 / 5 / 2 = 393MHz
- C6678EVM: 100MHz * 32 / 5 /2 = 320MHz

I think I should set the following parameters if I hope CPU speed is 1000MHz on C6678EVM. Is my understanding correct?

 sw_pll_prediv = 2 (1+1)
 sw_pll_mult = 40 (39+1)
 sw_pll_postdiv = 2 (1+1)
 sw_pll_flags = 1

Regards,
Kazu

  • Kazu,

    Yes, your understanding is correct. The nysh.map file provided on that forum post was created on a board where the OSCIN =312.5.

    For the EVM that has OSCIN 100Mhz, the multipliers would need to be configured as you specified here:

    Kazu Kon said:
     sw_pll_prediv = 2 (1+1)
     sw_pll_mult = 40 (39+1)
     sw_pll_postdiv = 2 (1+1)
     sw_pll_flags = 1

    This aligns with the table 2-24 provided in the C6678 datasheet.

    Regards,

    Rahul