Hi,
I am working on CCS V5.4.0.00091, mcsdk V3.00.00.11, pdk V1.00.00.11.
I need Lte Viterbi decoder(VCP2) project for keystone 2 6638/6636 EVM. Kindly provide the same asap.
Thanks and Regards,
Shabrin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am working on CCS V5.4.0.00091, mcsdk V3.00.00.11, pdk V1.00.00.11.
I need Lte Viterbi decoder(VCP2) project for keystone 2 6638/6636 EVM. Kindly provide the same asap.
Thanks and Regards,
Shabrin
Hi Shabrin,
We don't have ready made CCS project for VCP2 peripheral but we do have drivers, you can create it.
Latest processor SDK:
C:\ti\pdk_k2hk_4_0_0\packages\ti\csl\src\ip\vcp2
MCSDK:
C:\ti\pdk_keystone2_3_01_04_07\packages\ti\csl\src\ip\vcp2
Please refer to this e2e discussion.

I would like to recommend to download the latest Processor SDK package for K2H (6638)

Hi Raja,
I am migrating VCP2 from keystone I to keystone II. I could see there are lot of changes done in csl_device.h file which is in k2h folder. I could see some macro definitions are missing in csl_device.h file. I wonder where this macro's are defined in keystone II architecture.
I am looking especially for these macros "CSL_INTC0_CPU_3_2_TPCCINT0, CSL_TPCC2_VCP0REVT, CSL_TPCC2_VCP0XEVT ". Could you please let me know in which file these macros are defined?
I am attaching csl_device.h files of both the architecture for reference. cslr_device_Keystone1.hcslr_device_Keystone2.h
Thanks and Regards,
Shabrin