Other Parts Discussed in Thread: TMS320DM8168
I am using my custom board based on TMS320DM8168, I want to boot from Nand using UBIFS. And I did as the 
said.At first I change the u-boot to support UBIFS.
I add the defines listed in the file, and make. unfortunately, it had errors.
And I change the other thing in the picture.
lucky,I make it. So I flash the u-boot.noxip.bin to the nand via u-boot and SD.
At last, the biggest problem come out. After the u-boot flashed into nand, and I can not reboot from nand. And I can see nothing from the uart.What should i do is booting from SD and erase the nand.
(I have tried to
#define (CONFIG_ENV_SIZE + (768 * 1024))
OR #define CONFIG_SYS_MALLOC_LEN (2 << 20)
OR #define CONFIG_SYS_MALLOC_LEN (4 << 20)
they all not work.)
can you tell me how to do with the UBIFS?