This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 cannot start with TPS650250

Other Parts Discussed in Thread: AM3352, TPS650250

Hello TI hardware team :

we are using am335x with ddr2 ,uboot  spl 2013.01.01 

Our product  meet the problem   .

It can not start up the uboot and linux about 10 in 100 PCBs.It is huge amount.

The uboot  spl only print one sentence  on serail line " U-Boot  SPL 2013.01.01"

,other 90% product behave normal ,the uboot and linux system run successfully.

We use TPS650250 to provide all the power to am3352 such as 1.26v to core and 1.35v to ddr.

We provide input power 5V to TPS650250 directly.

We found that from 4.7v to 5.3 v the bad PCBs can not start ,

but when input is 4.4v to 4.6v  and higher than 5.3v about5.4v  5.5 ,the uboot spl on the bad PCBs startup correctly ,and product function is fine.

The normal input power to our product is 5V .

Can you give some advice to us ? 

It is big problem to our company.Our project  which intend to use am335x is paused because of this problem,