Hi,
I have questions about AM572x.
Q1.There are three OPP mode(OPP_NOM, OPP_OD, OPP_HIGH).
Is it allow to disalbe the AVS and fix the OPP mode to OPP_NOM?
Q2.In AM572x EVM and IDK EVM schematics, DDR3L data bus layout seems wrong.
For example, in AM572x EVM schematics(TI_AM572XEVM_REV_A3.pdf) page.21
DDR1_D10(AM572x) are connected to DQ15(DDR3L Memory).
Other DDR3 data bus connection seems wrong also.
Is this typo of schematics?
Q3.In AM572x datasheet(sprs953) page.201 "Table 6-3 OSC0 Input Clock Electrical Characteristics",
the description of Iin seems wrong.
It said "Input current(3.3V mode)". I guess OSC0 Input current only support 1.8V.
Is it typo of datasheet?
Q4.My customer are planning to use external oscillator for OSC0 and its output Rise/Fall Time(10% to 90%) Max 6ns.
Are there spec of AM572x OSC0 which prescribe Rise/Fall time of 10% to 90%?
best regards,
g.f.