Hello Community,
Am335x Starter kit - has an un-populated header under the name of ZigBee which is actually SPI-0 Interface and can be used to boot load Starter Kit.
So i have a few Questions
- As SPI interface is fully configurable so what configuration i must consider before interfacing external SPI Flash ? or the Starter Kit by default support Dual SPI interfacein master configuration. i.e D0 (I/O-1) and D1(I/O-0) can be configured but which one is by default MOSI and MISO ?
- What is the most appropriate way to Boot Load SPI Flashinterfaced with Starter Kit Am335x processor ?
- There is a forum thread that says ..... https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/345773
" The CCS/JTAG does not perform external flash programming of any kind, as the number of flash IC vendors and the possible combinations of interfaces (SPI, parallel, I2C, etc.) and the physical arrangement varies greatly from board to board."
and another forum says you can only boot load external flash by using on-board Micro USB (XDS100v2) or Ethernet Interface.
On the Other hand i want to remove the on-board Micro USB (XDS100v2) and instead want to use external JTAG emulator (XDS100v2 or XDS510+) for SPI Flashing and Boot loading.
Is there any way around to use JTAG for this purpose?
or
The additional USB 2.0 and Uart Interfaces present in on-board Micro USB programming interface (XDS100v2) are being used while Flashing and Boot loading the SPI ?
Your Help is much appreciated....!
Thanks.