Hello,
We are trying to load XEM4 binary on IPU2 core from U-boot using early boot functionality. We are using GLSDK 6_04 U-boot to do the same.
We tried loading 'dra7-ipu2-fw.xem4' from U-boot and were able to connect to IPU2 core after stopping at U-boot using CCS. But, when we try to load any other XEM4 binary built by us on IPU2 core, we are getting the below error messages
find_resource_table: failed to get resource section header
spl_boot_ipu: failed to find resource table
and loading XEM4 binary fails.
We want to know about the following things:
1. How can we build XEM4 binary (SYSBIOS or Starter ware) having the resource table linked to the executable binary?
2. Is there a way to bypass finding the resource table in U-boot and successfully load the XEM4 binary on IPU2/IPU1 core from U-boot?
Thanks & Regards,
Shubham