Other Parts Discussed in Thread: TVP5158
Hi
I am using DM6467 and TVP5158 ,I want to connect 4-way TVP5158 to DM6467.Two TVP5158 cascade,Respectively,through the BT656 to connect to the DM6467's A and B ports.I'm using TVP5158 patch v02.01.17,when I opened A and B ports,DM6467 only can use one prot A or B port.Now I continue to read code,understand the code structure.I also would like too ask my proposal is feasible.