This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x: Warm Reset fails

Hi everyone,

We have one very strange issue: When we reboot our DM814x-based custom board via software warm reset it happens on very rare occasions, that the booting fails.

Our normal boot order is: UART, NAND-SPI, NAND. So when the board boots the "CCCC..." are coming at first. After that the device is booted via u-boot from NAND.

In the above mentioned error case, it is not booting at all, meaning even the "CCCC..." are NOT coming. Connecting via JTAG in that state also fails with a "Requested operation failed for security violation" error message in CCS (v6.1.1).

We already checked all power lines and everything seems fine. The only way to recover is power-off / power-on.

Anyone else having this issue or any hints for its reason?

Greetings,
Thomas.