This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x SPI Slave driver for Linux



Hi there,

My customer need to config SPI as slave mode on Beaglebone Black.
I did some research, there is a MS bit for SPI register can config SP as Master / Slave mode.
However, accroding to these E2E thread, the SPI slave driver is not support in TI SDK.
e2e.ti.com/.../1018003
e2e.ti.com/.../347177
These thread was create 2/3 years ago, I want to know if TI support SPI slave driver right now?
If yes, where can I find SPI slave driver for Beaglebone Black or AM335x EVM?
If no, is there any success case or demo code can help customer's development?

Thannk you.

BR,
Wayne Kuo