Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO
I met the following problems when testing OMAP-L137 PSP UART EDMA example
“..\pspdrivers_01_20_00\packages\ti\pspiom\examples\evmOMAPL137\uart\edma”
Problem #1: When I open the project file, a window pops out with the following error message:
"Project Update
CRegistryInfo::GetSABiosConfig() could not find ConfigSuffix"
Problem #2: When I compiled the code, I got the following error message:
--------------------------- uartSample.pjt - Debug ---------------------------
Error, Don't know how to build file "C:\Program Files\Texas Instruments\pspdrivers_01_20_00\packages\ti\pspiom\examples\evmOMAPL137\uart_copy\edma\build\uartSample.tcf"
[uartSample.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -pdr -fr"C:/Program Files/Texas Instruments/pspdrivers_01_20_00/packages/ti/pspiom/examples/evmOMAPL137/uart_copy/edma/build/Debug" -i"C:/Program Files/Texas Instruments/pspdrivers_01_20_00/packages/ti/pspiom/examples/evmOMAPL137/uart_copy/edma/build/../../../../../../../" -i"C:/Program Files/Texas Instruments/edma3_lld_01_06_00_01/packages" -i"C:/CCStudio_v3.3/bios_5_33_05/packages/ti/bios/include" -i"C:/CCStudio_v3.3/C6000/cgtools/include" -mv6740 -@"../build/Debug.lkf" "uartSample.c"
[Linking...] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
"C:\Users\Sean\AppData\Local\Temp\024923", line 14: fatal error: unrecognized
file: "C:\\Program Files\\Texas
Instruments\\pspdrivers_01_20_00\\packages\\ti\\pspiom\\examples\\evmOMAPL13
7\\uart_copy\\edma\\build\\uartSamplecfg.cmd"
>> Compilation failure
Build Complete,
3 Errors, 0 Warnings, 0 Remarks.
Could anybody please give me some advice how to fix them? Thank you.