This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I import makefile project into CCS according to below link, but is doesn't recognize the project as below snapshot:
Garrett,
#1. Is this makefile under IPC differents with CCS generated makefile?
#2. When I import the makefile into CCS, it doens't recognize it.
#3. We can execute the IPC makefile in Win7 command line or in CCS command line, no need to under Linux, but why can't import to CCS?
#4. I can't open the URL () in your provided URL, from the case in your URL, seems it create a new CCS makefile project with existing code. in this way, if add new code or folder into the project, need to create new project again? if so, it is not convenient.