This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x kernel panic

Hi,

My customer made own board based on AM437x starter kit.

When customer tried to boot from SD card, Karnel panic occurred.

The below is boot log.

---------------------------------------------

・[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.1.6-g52c4aa7 (root@ubuntu-VirtualBox) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #3 PREEMPT Tue Dec 6 18:17:41 JST 2016
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM437x SK EVM
[    0.000000] cma: Reserved 24 MiB at 0xbe800000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM437x ES1.2 (neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260434
[    0.000000] Kernel command line: console=ttyO0,115200n8 video=HDMI-A-1:800x600 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 1004580K/1048576K available (6263K kernel code, 261K rwdata, 2104K rodata, 268K init, 231K bss, 19420K reserved, 24576K cma-reserved, 245760K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc083405c   (8369 kB)
[    0.000000]       .init : 0xc0835000 - 0xc0878000   ( 268 kB)
[    0.000000]       .data : 0xc0878000 - 0xc08b9468   ( 262 kB)
[    0.000000]        .bss : 0xc08bc000 - 0xc08f5c38   ( 232 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Additional per-CPU info printed with stalls.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L2C: platform modifies aux control register: 0x0e030000 -> 0x3e430000
[    0.000000] L2C: DT/platform modifies aux control register: 0x0e030000 -> 0x3e430000
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] OMAP L2C310: ROM does not support power control setting
[    0.000000] L2C-310 ID prefetch enabled, offset 1 lines
[    0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x7e430000
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000011] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000027] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.000036] OMAP clocksource: timer1 at 24000000 Hz
[    0.000172] Console: colour dummy device 80x30
[    0.000195] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[    0.000200] This ensures that you still see kernel messages. Please
[    0.000204] update your kernel commandline.
[    0.000220] Calibrating delay loop... 1993.93 BogoMIPS (lpj=9969664)
[    0.059325] pid_max: default: 32768 minimum: 301
[    0.059421] Security Framework initialized
[    0.059460] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.059469] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.060106] Initializing cgroup subsys blkio
[    0.060128] Initializing cgroup subsys memory
[    0.060175] Initializing cgroup subsys devices
[    0.060190] Initializing cgroup subsys freezer
[    0.060203] Initializing cgroup subsys perf_event
[    0.060230] CPU: Testing write buffer coherency: ok
[    0.060569] Setting up static identity map for 0x80008200 - 0x80008270
[    0.062042] devtmpfs: initialized
[    0.070996] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.081964] omap_hwmod: tptc0 using broken dt data from edma
[    0.082073] omap_hwmod: tptc1 using broken dt data from edma
[    0.082162] omap_hwmod: tptc2 using broken dt data from edma
[    0.149017] omap_hwmod: rtc: _wait_target_disable failed
[    0.149349] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.151084] pinctrl core: initialized pinctrl subsystem
[    0.152145] NET: Registered protocol family 16
[    0.153412] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.179369] cpuidle: using governor ladder
[    0.209359] cpuidle: using governor menu
[    0.209734] of_device_add soc
[    0.209886] of_device_add soc:mpu
[    0.210078] of_device_add 48241000.interrupt-controller
[    0.210206] of_device_add 48281000.interrupt-controller
[    0.210319] of_device_add 48242000.l2-cache-controller
[    0.210492] of_device_add 44000000.ocp
[    0.210757] omap_l3_noc 44000000.ocp: L3 debug error: target 8 mod:0 (unclearable)
[    0.210778] omap_l3_noc 44000000.ocp: L3 debug error: target 13 mod:1 (unclearable)
[    0.210817] omap_l3_noc 44000000.ocp: L3 application error: target 8 mod:0 (unclearable)
[    0.210830] ------------[ cut here ]------------
[    0.210848] WARNING: CPU: 0 PID: 1 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x220/0x34c()
[    0.210856] 44000000.ocp:L3 Custom Error: MASTER M2 (64-bit) TARGET L4_WKUP (Read): Data Access in User mode during Functional access
[    0.210862] Modules linked in:
[    0.210877] CPU: 0 PID: 1 Comm: swapper Not tainted 4.1.6-g52c4aa7 #3
[    0.210883] Hardware name: Generic AM43 (Flattened Device Tree)
[    0.210889] Backtrace:
[    0.210916] [<c0012b70>] (dump_backtrace) from [<c0012d90>] (show_stack+0x18/0x1c)
[    0.210921]  r7:c07b3f0c r6:00000093 r5:00000009 r4:00000000
[    0.210944] [<c0012d78>] (show_stack) from [<c061d190>] (dump_stack+0x20/0x28)
[    0.210962] [<c061d170>] (dump_stack) from [<c0039e60>] (warn_slowpath_common+0x7c/0xb4)
[    0.210973] [<c0039de4>] (warn_slowpath_common) from [<c0039ed0>] (warn_slowpath_fmt+0x38/0x40)
[    0.210978]  r8:c07b3f94 r7:c0652d88 r6:ee8de4d0 r5:c07b3e38 r4:c07b3edc
[    0.210996] [<c0039e9c>] (warn_slowpath_fmt) from [<c030c4c8>] (l3_interrupt_handler+0x220/0x34c)
[    0.211000]  r3:ee8de2c0 r2:c07b3edc
[    0.211007]  r4:80080003
[    0.211023] [<c030c2a8>] (l3_interrupt_handler) from [<c006c748>] (handle_irq_event_percpu+0x7c/0x148)
[    0.211028]  r10:c08b8c5b r9:ee8da840 r8:00000013 r7:00000000 r6:00000000 r5:ee8de840
[    0.211042]  r4:ee8de840
[    0.211053] [<c006c6cc>] (handle_irq_event_percpu) from [<c006c87c>] (handle_irq_event+0x68/0x90)
[    0.211057]  r10:00000013 r9:00000000 r8:ee808000 r7:00000001 r6:00000000 r5:ee8de840
[    0.211070]  r4:ee8da840
[    0.211083] [<c006c814>] (handle_irq_event) from [<c006f200>] (handle_fasteoi_irq+0xb8/0x1e8)
[    0.211088]  r5:c087f480 r4:ee8da840
[    0.211101] [<c006f148>] (handle_fasteoi_irq) from [<c006be70>] (generic_handle_irq+0x30/0x44)
[    0.211106]  r5:c089321c r4:00000013
[    0.211118] [<c006be40>] (generic_handle_irq) from [<c006c0d0>] (__handle_domain_irq+0x50/0xb0)
[    0.211123]  r5:c089321c r4:00000013
[    0.211135] [<c006c080>] (__handle_domain_irq) from [<c00094a8>] (gic_handle_irq+0x28/0x60)
[    0.211139]  r9:00000000 r8:60000113 r7:fa240100 r6:c087a48c r5:ee863ba8 r4:fa24010c
[    0.211163] [<c0009480>] (gic_handle_irq) from [<c06225c0>] (__irq_svc+0x40/0x74)
[    0.211170] Exception stack(0xee863ba8 to 0xee863bf0)
[    0.211178] 3ba0:                   ee8da840 ee8de840 00000000 00000000 ee8da840 ee8de840
[    0.211187] 3bc0: ee8da840 00000013 60000113 00000000 00000013 ee863c1c ee863bf0 ee863bf0
[    0.211194] 3be0: c006dd3c c006db94 60000113 ffffffff
[    0.211198]  r7:ee863bdc r6:ffffffff r5:60000113 r4:c006db94
[    0.211214] [<c006d914>] (__setup_irq) from [<c006e004>] (request_threaded_irq+0xc4/0x154)
[    0.211219]  r9:00000000 r8:ee8de4d0 r7:c030c2a8 r6:ee8da840 r5:00000000 r4:ee8de840
[    0.211239] [<c006df40>] (request_threaded_irq) from [<c0070200>] (devm_request_threaded_irq+0x5c/0xa4)
[    0.211244]  r10:00000002 r9:ee8d9e10 r8:00000000 r7:00000013 r6:ee8de4d0 r5:ee8de810
[    0.211256]  r4:c030c2a8 r3:00000000
[    0.211269] [<c00701a4>] (devm_request_threaded_irq) from [<c030c1f8>] (omap_l3_probe+0x1cc/0x27c)
[    0.211274]  r9:ee8de4d0 r8:ee8d9e10 r7:c08e50f4 r6:ee8de4d0 r5:c08e50f4 r4:00000000
[    0.211297] [<c030c02c>] (omap_l3_probe) from [<c0406934>] (platform_drv_probe+0x4c/0xac)
[    0.211302]  r10:00000000 r9:00000000 r8:00000000 r7:fffffdfb r6:c08937ac r5:ee8d9e10
[    0.211314]  r4:c08ed1c0
[    0.211325] [<c04068e8>] (platform_drv_probe) from [<c0404f30>] (driver_probe_device+0x17c/0x2c0)
[    0.211330]  r7:c08937ac r6:00000000 r5:ee8d9e10 r4:c08ed1c0
[    0.211344] [<c0404db4>] (driver_probe_device) from [<c04050bc>] (__device_attach+0x48/0x4c)
[    0.211349]  r9:00000000 r8:c08ed19c r7:00000000 r6:c0405074 r5:ee8d9e10 r4:c08937ac
[    0.211378] [<c0405074>] (__device_attach) from [<c0403348>] (bus_for_each_drv+0x6c/0xa0)
[    0.211383]  r5:ee8d9e10 r4:00000000
[    0.211395] [<c04032dc>] (bus_for_each_drv) from [<c0404d74>] (device_attach+0x78/0x90)
[    0.211399]  r6:ee8d9e44 r5:ee8d9e10 r4:ee8d9e10
[    0.211412] [<c0404cfc>] (device_attach) from [<c04043d0>] (bus_probe_device+0x8c/0xb4)
[    0.211416]  r7:00000000 r6:c08a0fa8 r5:ee8d9e10 r4:ee8d9e18
[    0.211432] [<c0404344>] (bus_probe_device) from [<c04024f4>] (device_add+0x3c4/0x570)
[    0.211436]  r7:00000000 r6:ee8d9e10 r5:c08a0e48 r4:ee8d9e18
[    0.211460] [<c0402130>] (device_add) from [<c04eb738>] (of_device_add+0x44/0x54)
[    0.211465]  r10:00000000 r9:00000000 r8:c0872c5c r7:ee8d9e10 r6:00000000 r5:eeed44fc
[    0.211477]  r4:ee8d9e00
[    0.211489] [<c04eb6f4>] (of_device_add) from [<c04ebf8c>] (of_platform_device_create_pdata+0x84/0xc8)
[    0.211493]  r5:eeed44fc r4:ee8d9e00
[    0.211506] [<c04ebf08>] (of_platform_device_create_pdata) from [<c04ec0d4>] (of_platform_bus_create+0xe8/0x194)
[    0.211511]  r7:00000001 r6:c086c1d8 r5:eeed44fc r4:00000000
[    0.211527] [<c04ebfec>] (of_platform_bus_create) from [<c04ec2bc>] (of_platform_populate+0x64/0xc0)
[    0.211531]  r10:00000000 r9:00000001 r8:00000000 r7:c086c1d8 r6:c0872c5c r5:eeed3450
[    0.211544]  r4:eeed44fc
[    0.211556] [<c04ec258>] (of_platform_populate) from [<c0844418>] (pdata_quirks_init+0x3c/0x4c)
[    0.211561]  r9:c086ac38 r8:c08bc000 r7:ee8dbcc0 r6:c087cc60 r5:c0872c5c r4:c086c1d0
[    0.211578] [<c08443dc>] (pdata_quirks_init) from [<c08443d0>] (omap_generic_init+0x18/0x24)
[    0.211582]  r5:c08387f4 r4:c087cc60
[    0.211594] [<c08443b8>] (omap_generic_init) from [<c083881c>] (customize_machine+0x28/0x4c)
[    0.211604] [<c08387f4>] (customize_machine) from [<c00096c4>] (do_one_initcall+0x88/0x1e0)
[    0.211625] [<c000963c>] (do_one_initcall) from [<c0835e78>] (kernel_init_freeable+0x178/0x240)
[    0.211630]  r10:c08355e8 r9:c086ac38 r8:c08bc000 r7:c0876be4 r6:c08bc000 r5:c086ac24
[    0.211643]  r4:00000003
[    0.211654] [<c0835d00>] (kernel_init_freeable) from [<c061a220>] (kernel_init+0x10/0xf4)
[    0.211659]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c061a210
[    0.211671]  r4:00000000
[    0.211684] [<c061a210>] (kernel_init) from [<c000f988>] (ret_from_fork+0x14/0x2c)
[    0.211688]  r5:c061a210 r4:00000000
[    0.211716] ---[ end trace 71a80298ab8eafc9 ]---
[    0.211735] omap_l3_noc 44000000.ocp: L3 application error: target 13 mod:1 (unclearable)
[    0.211820] of_device_add 44000000.ocp:l4_wkup@44c00000
[    0.211986] of_device_add 44d00000.wkup_m3
[    0.212176] of_device_add 44df0000.prcm
[    0.212297] of_device_add 44e10000.scm
[    0.212428] of_device_add 44e10800.pinmux
[    0.212545] of_device_add 44e10000.scm_conf
[    0.212699] of_device_add 44e11324.wkup_m3_ipc
[    0.212816] of_device_add 4c000000.emif
[    0.213022] of_device_add 49000000.edma
[    0.213219] of_device_add 48022000.serial
[    0.213403] of_device_add 480c8000.mailbox
[    0.213590] of_device_add 44e86000.counter
[    0.213782] of_device_add 44e3e000.rtc
[    0.213961] of_device_add 44e35000.wdt
[    0.214135] of_device_add 44e07000.gpio
[    0.214575] OMAP GPIO hardware version 0.1
[    0.214827] of_device_add 4804c000.gpio
[    0.215399] of_device_add 48322000.gpio
[    0.215893] of_device_add 480ca000.spinlock
[    0.216177] of_device_add 44e0b000.i2c
[    0.216382] of_device_add 4802a000.i2c
[    0.216571] of_device_add 48060000.mmc
[    0.216825] of_device_add 4a100000.ethernet
[    0.216980] of_device_add 48300000.epwmss
[    0.217211] of_device_add 53100000.sham
[    0.217383] of_device_add 53501000.aes
[    0.217540] of_device_add 53701000.des
[    0.217689] of_device_add 56000000.sgx
[    0.217854] of_device_add 48310000.rng
[    0.218112] of_device_add 54400000.pruss
[    0.218259] of_device_add 4803c000.mcasp
[    0.218425] of_device_add 48080000.elm
[    0.218571] of_device_add 44e10620.control-phy
[    0.218680] of_device_add 44e10628.control-phy
[    0.218778] of_device_add 44000000.ocp:ocp2scp@483a8000
[    0.218912] of_device_add 44000000.ocp:ocp2scp@483e8000
[    0.219090] of_device_add 48380000.omap_dwc3
[    0.219242] of_device_add 483c0000.omap_dwc3
[    0.219621] of_device_add 47900000.qspi
[    0.219812] of_device_add 4832a000.dss
[    0.219993] of_device_add 40300000.ocmcram
[    0.220230] of_device_add 48326000.vpfe
[    0.220367] of_device_add backlight
[    0.220468] of_device_add sound
[    0.220577] of_device_add matrix_keypad@0
[    0.220667] of_device_add leds
[    0.220755] of_device_add display
[    0.221438] of_device_add 4832a400.dispc
[    0.221877] No ATAGs?
[    0.221904] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.221911] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.255791] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[    0.258241] vgaarb: loaded
[    0.258671] SCSI subsystem initialized
[    0.259146] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c0_pins, deferring probe
[    0.259191] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins, deferring probe
[    0.259316] pps_core: LinuxPPS API ver. 1 registered
[    0.259323] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.259433] PTP clock support registered
[    0.260074] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.260310] Advanced Linux Sound Architecture Driver Initialized.
[    0.260944] Switched to clocksource timer1
[    0.268749] NET: Registered protocol family 2
[    0.269500] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.269574] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.269647] TCP: Hash tables configured (established 8192 bind 8192)
[    0.269793] UDP hash table entries: 512 (order: 1, 8192 bytes)
[    0.269814] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
[    0.269970] NET: Registered protocol family 1
[    0.270288] RPC: Registered named UNIX socket transport module.
[    0.270299] RPC: Registered udp transport module.
[    0.270304] RPC: Registered tcp transport module.
[    0.270309] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.272159] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.272236] audit: initializing netlink subsys (disabled)
[    0.272286] audit: type=2000 audit(0.260:1): initialized
[    0.277462] VFS: Disk quotas dquot_6.6.0
[    0.277638] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.279197] NFS: Registering the id_resolver key type
[    0.279249] Key type id_resolver registered
[    0.279258] Key type id_legacy registered
[    0.279322] jffs2: version 2.2. (NAND) (SUMMARY)  c 2001-2006 Red Hat, Inc.
[    0.281588] NET: Registered protocol family 38
[    0.281679] bounce: pool size: 64 pages
[    0.281694] io scheduler noop registered
[    0.281705] io scheduler deadline registered
[    0.281763] io scheduler cfq registered (default)
[    0.282082] of_device_add 483a8000.phy
[    0.282390] of_device_add 483e8000.phy
[    0.283415] pinctrl-single 44e10800.pinmux: 199 pins at pa f9e10800 size 796
[    0.284044] of_device_add 48300100.ecap
[    0.285178] backlight supply power not found, using dummy regulator
[    0.286635] 4832a000.dss supply vdda_video not found, using dummy regulator
[    0.286758] OMAP DSS rev 2.0
[    0.287072] omapdss_dss 4832a000.dss: bound 4832a400.dispc (ops dispc_component_ops)
[    0.288743] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[    0.289583] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.292067] omap8250 48022000.serial: No clock speed specified: using default: 48000000
[    0.292496] 48022000.serial: ttyS0 at MMIO 0x48022000 (irq = 25, base_baud = 3000000) is a 8250
[    1.816153] console [ttyS0] enabled
[    1.820521] [drm] Initialized drm 1.1.0 20060810
[    1.835142] brd: module loaded
[    1.842738] loop: module loaded
[    1.846701] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.855291] mousedev: PS/2 mouse device common for all mice
[    1.860876] i2c /dev entries driver
[    1.865341] omap_hsmmc 48060000.mmc: Got CD GPIO
[    1.891342] ledtrig-cpu: registered to indicate activity on CPUs
[    1.897603] omap-aes 53501000.aes: OMAP AES hw accel rev: 0.1
[    1.904409] omap-des 53701000.des: OMAP DES hw accel rev: 0.33
[    1.911308] omap-sham 53100000.sham: hw accel on OMAP rev 0.0
[    1.918833]  remoteproc0: wkup_m3 is available
[    1.923450]  remoteproc0: Note: remoteproc is still under development and considered experimental.
[    1.932542]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[    1.943039]  remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
[    1.953768] oprofile: no performance counters
[    1.958226] oprofile: using timer interrupt.
[    1.962641]  remoteproc0: Falling back to user helper
[    1.968074] Initializing XFRM netlink socket
[    1.972450] NET: Registered protocol family 17
[    1.976921] NET: Registered protocol family 15
[    1.981484] Key type dns_resolver registered
[    1.985915] omap_voltage_late_init: Voltage driver support not added
[    1.992706] ThumbEE CPU extension supported.
[    1.996989] Registering SWP/SWPB emulation handler
[    2.004125] omapdrm omapdrm.0: DMM not available, disable DMM support
[    2.011427] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    2.018038] [drm] No driver support for vblank timestamp query.
[    2.063725] Console: switching to colour frame buffer device 60x34
[    2.086601] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[    2.092523] omapdrm omapdrm.0: registered panic notifier
[    2.120978] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[    2.143249] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc1
[    2.151678] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc2
[    2.159092] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc3
[    2.168300] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc4
[    2.175720] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc5
[    2.183728] of_device_add 44e0b000.i2c:tps@24:regulator-dcdc6
[    2.191252] of_device_add 44e0b000.i2c:tps@24:regulator-ldo1
[    2.199464] of_device_add 44e0b000.i2c:tps@24:power-button
[    2.205519] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz
[    2.212456] omap_i2c 4802a000.i2c: bus 1 rev0.12 at 400 kHz
[    2.219077] omap_hsmmc 48060000.mmc: Got CD GPIO
[    2.262035] of_device_add 4a101000.mdio
[    2.320969] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    2.327062] davinci_mdio 4a101000.mdio: detected phy mask ffffff3f
[    2.334556] libphy: 4a101000.mdio: probed
[    2.338576] davinci_mdio 4a101000.mdio: phy[6]: device 4a101000.mdio:06, driver unknown
[    2.346650] davinci_mdio 4a101000.mdio: phy[7]: device 4a101000.mdio:07, driver unknown
[    2.354791] of_device_add 44e10650.cpsw-phy-sel
[    2.359977] cpsw 4a100000.ethernet: Detected MACID = a0:f6:fd:6d:f0:a5
[    2.367436] cpsw 4a100000.ethernet: cpsw: Detected MACID = a0:f6:fd:6d:f0:a7
[    2.375364] hctosys: unable to open rtc device (rtc0)
[    2.384234] ALSA device list:
[    2.387289] mmc0: host does not support reading read-only switch, assuming write-enable
[    2.395378]   No soundcards found.
[    2.399268] Waiting for root device PARTUUID=00000000-02...
[    2.409207] mmc0: new high speed SDHC card at address e624
[    2.415209] mmcblk0: mmc0:e624 SU08G 7.40 GiB
[    2.421344]  mmcblk0: p1 p2
[    2.544262] EXT4-fs (mmcblk0p2): recovery complete
[    2.549070] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.557272] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.567244] devtmpfs: mounted
[    2.570684] Freeing unused kernel memory: 268K (c0835000 - c0878000)
[    2.615602] Unhandled fault: imprecise external abort (0x1406) at 0xb6f06888
[    2.622649] pgd = ee03c000
[    2.625346] [b6f06888] *pgd=ae01a831, *pte=be00e34f, *ppte=be00e83f
[    2.631988] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000007
[    2.631988]
[    2.641110] drm_kms_helper: panic occurred, switching back to text console
[    2.647995] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000007
[    2.647995]

----------------------------------------------

According to my customer's info, kernel panic is occurred in "of_device_add()" in drivers/ of/device.c while Linux Init.

Why does karnel panic occur? Please give me some advices.

I appreciate your quick reply.

Best regards,

Michi