This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x processor family - Telematics Device Hang issue.

Hi ,

Pls find details of the project :-

  1. We are developing Telematics device along with infotainment feature.
  2. We are using DRA604 and Arago Linux.
  3. Around 10 exe are running on the system.Some are related with Telematics Application and some are with Infotainment.

We are facing one issue and details are:-

  1. When we keep the system for long run of test (Approx. 2-5 days) then at any point system hang.
  2. System is not recovering from hang condition by itself.
  3. We have to hard reset the system.
  4. Same issue is observed with single test application as well as integrated Application.
  5. Same issue faced during onbench and vehicle level test.