This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5716: AVS setting for IVA and GPU

Genius 5785 points
Part Number: AM5716
Other Parts Discussed in Thread: AM5718

Hello,

I'll use AM5716 which does not have IVA (and GPU). The OS is Linux.

Please tell me about the setting of AVS for IVA. Do the following registers contain valid values?
CTRL_CORE_STD_FUSE_OPP_VMIN_IVA_2 [11: 0] STD_FUSE_OPP_VMIN_IVA_ 2

Also please tell me about TRM "Figure 18-13. AVS Class 0 Procedure". Should I skip IVA branch? If I chose 'NO'(skip), I think the voltage of VDD_IVA will remain at default 1.06 V. Or, can I set AVS based on the setting value of the above register? If I can do it, I can expect a little power saving and share the source code for AVS procedure between AM5718 and AM5716.

Regards,
Kazu