Hello TI staff,
Beside my problems of setting the PLLs, I have met a spurious problem which did not occur before : the power and sleep controller for modules presents some infinite setup time.
Let me explain:
In my GEL file I have a Setup_Psc_All() procedure, that I made carefully not to set the reserved modules (as on evm files on few reserved modules which is problematic).
I followed the procedure explained on the ARM subsystem Datasheet.
And I got an infinite time/loop: on watching that the state has gone to the requested state in the MDSTAT register.
When I meet a problematic module, I remove it and then the 'error' propagates to the next one.
My procedure is here for information:
Any help is welcome.
----------------------------------------------------
/* ------------------------------------------------------------------------ *
* *
* Setup_Psc_All_On( ) *
* Enable all non-reserved power modules. *
* *
* ------------------------------------------------------------------------ */
Setup_Psc_All_On( )
{
unsigned char i=0;
unsigned char lpsc_start;
unsigned char lpsc_end,lpscgroup,lpscmin,lpscmax;
lpscmin =0;
lpscmax =3;
GEL_TextOut( "Setup Power Modules (All on)... " );
for(lpscgroup=lpscmin ; lpscgroup <=lpscmax; lpscgroup++)
{
if(lpscgroup==0)
{
lpsc_start = 0; // Enabling LPSC 0 to 15 SCR first
lpsc_end = 15;
}
else if(lpscgroup==1)
{/* Skip reserved LPSCs 16 */
lpsc_start = 17; // Enabling LPSC 17 to 28 SCR first
lpsc_end = 28;
}
else if (lpscgroup == 2)
{ /* Skip locked =(Always on or reserved) LPSCs [29-37] */
lpsc_start = 38;
lpsc_end = 47;
}
else
{
lpsc_start = 50;
lpsc_end = 51;
}
//state=0x3=Enable LPSC's
for(i=lpsc_start; i<=lpsc_end; i++)
{
GEL_TextOut( "Module i= %d... ",,,,,i );
psc_change_state( i , 3 );
}
}
GEL_TextOut("\nDM365 all Module Clocks are Turned on\n");
}
/* ------------------------------------------------------------------------ *
* *
* psc_change_state( id, state ) *
* id = Domain #ID *
* state = ( ENABLE, DISABLE, SYNCRESET, RESET ) *
* ( =3 , =2 , =1 , =0 ) *
* *
* ------------------------------------------------------------------------ */
psc_change_state( int id, int state )
{
int* mdstat = ( int* )( 0x01c41800 + ( 4 * id ) );
int* mdctl = ( int* )( 0x01c41a00 + ( 4 * id ) );
int set_interrupt;
/*
* Step 0 - Ignore request if the state is already set as is
*/
if ( ( ( *mdstat ) & 0x1f ) == state )
return;
/*
* Step 1 - Wait for PTSTAT.GOSTAT to clear = previous transitions must finish
*/
while( PSC_PTSTAT & 1 )
{
GEL_TextOut( "waiting PTSTAT for %d... ",,,,,id );
};
/*
* Step 2 - Set MDCTLx.NEXT to new state
*/
*mdctl &= ~0x1f;
*mdctl |= state;
/*
* Step 3 - Start power transition ( set PTCMD.GO to 1 )
*/
PSC_PTCMD |= 1;
/*
* Step 4 - Wait for PTSTAT.GOSTAT to clear
*/
while( PSC_PTSTAT & 1 )
{
GEL_TextOut( "waiting PTSTAT for %d... ",,,,,id );
};
/*
* Step 5 - Wait for MDSTAT to be set to requested state
*/
while ( (*mdstat)&0x1f != state )
{
GEL_TextOut( "waiting MDSTAT for %d go for %d... ",,,,,id,state );
};
}
----------------------------------------------------------------------------------------------