This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Keystone 2 SRIO Input Retry Stopped Error

Hi,

We are working on interfacing SRIO communication between FPGA and Keystone 2 Processor.

Config Details

Link Speed - 5Gbps per port,

Port Mode - 4X

NWrite packet

In our setup, the FPGA GTX Transreceivers are directly connected to the DSP SRIO Serdes lanes.

The SRIO code is initialized on the DSP core 0 of the Keystone 2 Processor.

Issue:

We are facing some issue while transferring data from FPGA to DSP. The DSP able to receive approximately 16MB of data from FPGA then it enter into Input Retry Stopped Error.

The Input Retry Stopped Error Bit keeps on Toggling on the DSP side.

The packet formation on the FPGA side also stopped due to packet stop at retry state request from DSP.

Similarly when we tested the same FPGA with Keystone 1 processor, data transferring working without any issue.

We tested the below scenarios where data transferring from FPGA to DSP working without any issue.

 

S.No

Setup Type

Status

Error

1

FPGA to Keystone 1 (Direct Connection )

Working

Continuous Streaming of Data

2

Keystone 2 to Keystone 2 (Direct Connection )

Working

Continuous Streaming of Data

3

FPGA (EVM setup ) to Keystone

Working

Continuous Streaming of Data

 

What is the difference in running SRIO on Keystone 1 and Keystone 2 ?

Please provide us the solution to solve this issue .

Thanks and Regards,

Narayan