Hi Champs,
One of my customer is trying the big endian TFTP boot on C6678EVM, but he can not. He has already done the little endian boot w/o any problems.
So, dose anyone have any validated examples for the boot for the EVM?
Regards,
j-breeze
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champs,
One of my customer is trying the big endian TFTP boot on C6678EVM, but he can not. He has already done the little endian boot w/o any problems.
So, dose anyone have any validated examples for the boot for the EVM?
Regards,
j-breeze
Hi Yordan,
Yes. My customer has compiled the IBL using a command below in MinGW environment.
make evm_c6678_i2c ENDIAN=big I2C_BUS_ADDR=0x51
Could you please let me know what I should check next?
Regards,
j-breeze
Hi Yordan,
My customer is trying to use BOOTP. So, dose the TFTP boot support BOOTP? Can I enable it like below?
replace
ibl.bootModes[2].u.ethBoot.doBootp = FALSE;
with
ibl.bootModes[2].u.ethBoot.doBootp = TRUE;
Regards,
j-breeze
Hi Yordan,
I am still expecting your response regarding the TFTP boot.
The below is my result.
----------------------------
| doBootp
Endian |-------------------
| FALSE | TRUE
--------+-------------------
Little | BOOT OK | BOOT NG
Big | BOOT OK | BOOT NG
----------------------------
Regards,
j-breeze
Hi,
The below is my latest result. I attached the Wireshark logs.
o Little Endian & BOOTP Enabled (file name: TFTP_BOOT_LE_BOOTP_ENA.pcapng)
- No.102: BOOTP Boot Request from 40:5f:c2:b8:fc:9a (TexasIns_b8:fc:9a)
- No.104: DHCP DHCP Offer - Transaction ID 0x1
- No.105: ARP Who has 192.168.2.3? Tell 192.168.2.201
- No.107: TFTP Read Request, File: app.out, Transfer type: octet
- No.109: TFTP Data Packet, Block: 1
- No.110: TFTP Acknowledgement, Block: 1
* TFTP BOOT OK!
o Big Endian & BOOTP Enabled (file name: TFTP_BOOT_BE_BOOTP_ENA.pcapng)
- No. 82: BOOTP Boot Request from 40:5f:c2:b8:fc:9a (TexasIns_b8:fc:9a)
- No. 83: DHCP DHCP Offer - Transaction ID 0x1
- No. 85 ARP Who has 192.168.2.101? Tell 192.168.2.3
- No.122: BOOTP Boot Request from 40:5f:c2:b8:fc:9a (TexasIns_b8:fc:9a)
- No.123: DHCP DHCP Offer - Transaction ID 0x1
- No.124 ARP Who has 192.168.2.101? Tell 192.168.2.3
- No.171: BOOTP Boot Request from 40:5f:c2:b8:fc:9a (TexasIns_b8:fc:9a)
- No.172: DHCP DHCP Offer - Transaction ID 0x1
- No.174: ARP Who has 192.168.2.101? Tell 192.168.2.3
* TFTP BOOT NG!
What is the reason for not working with Big Endian?
Any comment would be appreciated.
TFTP_BOOT_BOOTP_ENA_Wireshark_Logs.zip
Regards,
j-breeze
HI,
I found that ARP was issued from PC(TFTP server), not the EVM when BOOTP was enabled in BE mode.
So, could you please let me know what part of the example code I should modify to issue ARP from the EVM?
Regards,
j-breeze
j-breeze,
Please check my responses here:
ALso refer to the attached document to run TFTP boot in BE mode. This was validated using MCSDK baseline. With Processor SDK RTOS, we have tested this in little endian mode only.
8637.How to test BOOTP C6678 EVM in BE mode.pdf
Regards,
Rahul
Hi Rahul,
Thank you for your support.
I think the document you attached is for ROM Ethernet Boot, not IBL TFTP Boot. Because the DEVSTAT value is 0x00001C84 and it shows ROM Ethernet Boot mode. Could you please check it out again?
And, could you please refer my Wireshark logs I attached in my previous post and let me clarify why ARP is issued from PC which I use for DHCP/TFTP server, not the EVM, when BOOTP is enabled in BE mode?
Regards,
j-breeze
Hi Rahul,
My customer has already built the IBL in BE mode as following. I think there is no problem.
make evm_c6678_i2c ENDIAN=big I2C_BUS_ADDR=0x51
Can I ask you to verify the boot and give me the Wireshark log?
Regards,
j-breeze
J-Breeze,
I have provided the Wireshark log from what I am seeing from the TFTP BOOTP based BE boot.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/IBL_5F00_TFTP_5F00_BE_5F00_WireShark_5F00_log.pcapng
I definitely see a response and the image transfer happening in big endian mode.
Regards,
Rahul
Hi Rahul,
Thank you so much for sharing your Wireshark log. Could you please tell me the following?
Q1) What type of data in a SDK did you use, pre-build or rebuild?
Q2) What tool did you use for servers for the verification on your PC?
Q3) What are settings of the tool?
Regards,
j-breeze
J-breeze,
I used the MCSDK images for this effort and used prebuilt binaries as I didn`t make any changes in the source.
I configured the boot parameter table using the i2cConfig.gel as described here:
Modified the GEL to enable BOOTP and ran the .out to flash the parameter table.
2. On the host I used a tool called TFTP32 which is described here:
I have attached the snapshot of the tool settings.:
To test this I used a switch that was not on my office network and the configured the machine LAN with static IP and connected it to the switch.
Hope this helps.
Regards,
Rahul
Hi Raul,
I really appreciate your support.
I have already use the tool and configured the table using the GEL file as you told me, but the boot dose not work yet in my environment.
I connect my PC to C6678EVM directly using cross cable. Is it wrong?
And, I found a difference b/w our Wireshark logs.
In your log, BOOTP/Boot Reply(No.2) is issued after BOOTP/Boot Request(No.1), and ARPs(No. 3 & 4) are issued, and then TFTP transfer starts.
On the other hand, DHCP/DHCP Offer(No.104) is issued after BOOTP/Boot Request(No.102), and ARPs(No. 105 & 106) are issued, and then TFTP transfer starts in my log(for little endian mode in which the boot work).
I'm not familier with the protocol. Could you please let me crarify the difference, if you have any?
Regards,
j-breeze
Rahul,
I'm looking at the IBL code, but I'm not sure why the boot dose not work.
Could you please advice me what are the possible causes for not issuing ARP in the BE mode in my configration?
Any comment would be really appreciated.
Regards,
j-breeze
J-Breeze,
Big endian mode is not very widely supported so I haven`t done a lot of debugging in this endian. Did you try to create a local connection using a switch as I mentioned or are you still connecting the PC directly to the EVM.
Regards,
Rahul
Hi Rahul,
I'm still connecting my PC directly to the EVM.
By the way, I'd like to ask you another question. I want to debug the IBL, especially bootp.c file.
So, could you please let me know how I can see mprintf() outputs below?
I'm not sure, but I guess that the Boot Reply/DHCP Offer packet is not interpreted correctly in the BE mode.
o bootp.c
(C:\ti\pdk_c667x_2_0_5\packages\ti\boot\ibl\src\driver\eth)
- Line 312~320
/* DEBUG Message: */
mprintf ("*****************************\n");
mprintf ("BOOTP Complete\n");
mprintf (" IP Address : 0x%x\n", ntohl(netmcb.net_device.ip_address));
mprintf (" Net Mask : 0x%x\n", subnetmask);
mprintf (" Default Router: 0x%x\n", defaultRouter);
mprintf (" Server IP : 0x%x\n", ntohl(serverIP));
mprintf (" File Name : %s\n", ptr_bootphdr->file);
mprintf ("*****************************\n");
Regards,
j-breeze
Hi Rahul,
I'd like to ask your advice about the IBL code.
I'm trying to debug the code and I found that it does not reach a bootp_receive() function after executing a bootp_tmr_expiry() function in bootp.c in the BE mode. Because of this, I can not see mprintf() outputs I mentioned in my previous post in the bootp_receive().
So, could you please give me some advice on the possible causes?
Regards,
j-breeze
Hi,
The below is my Tftpd64 log. I hope It would be useful information.
o LE
Rcvd BootP Msg for IP 0.0.0.0, Mac 40:5F:C2:B8:FC:9A [08/06 15:50:43.155]
BOOTP: proposed address 192.168.2.201 [08/06 15:50:43.155]
Connection received from 192.168.2.201 on port 1234 [08/06 15:50:43.171]
Read request for file <app.out>. Mode octet [08/06 15:50:43.171]
Using local port 49175 [08/06 15:50:43.171]
<app.out>: sent 994 blks, 508780 bytes in 0 s. 0 blk resent [08/06 15:50:43.405]
Warning : received duplicated request from : [08/06 15:50:43.405]
Connection received from 192.168.2.201 on port 1234 [08/06 15:50:43.663]
Read request for file <app.out>. Mode octet [08/06 15:50:43.663]
Using local port 50022 [08/06 15:50:43.663]
<app.out>: sent 994 blks, 508780 bytes in 0 s. 0 blk resent [08/06 15:50:43.881]
o BE
Rcvd BootP Msg for IP 0.0.0.0, Mac 40:5F:C2:B8:FC:9A [08/06 15:57:01.839]
BOOTP: proposed address 192.168.2.201 [08/06 15:57:01.839]
Rcvd BootP Msg for IP 0.0.0.0, Mac 40:5F:C2:B8:FC:9A [08/06 15:57:09.808]
BOOTP: proposed address 192.168.2.201 [08/06 15:57:09.808]
Rcvd BootP Msg for IP 0.0.0.0, Mac 40:5F:C2:B8:FC:9A [08/06 15:57:21.764]
BOOTP: proposed address 192.168.2.201 [08/06 15:57:21.764]
.
.
.
Regards,
j-breeze
Hi Champs,
Dose anyone help me? I have not been solved yet.
The IBL in BE mode repeats a if statement in arp_resplve() below and then excutes another if statement that shows an error "BOOTP Failure: Max Retransmissions exceeded". What could be wrong with it? What should I check next?
Any comment would be appreciated.
o arp.c
(C:\ti\pdk_c667x_2_0_5\packages\ti\boot\ibl\src\driver\eth)
- Line 127~142
/* Special Case: Are we sending the packet to 255.255.255.255? */
if (dst_ip == (IPN)0xFFFFFFFF)
{
/* YES. This implies that the destination MAC Address in the packet is the Broadcast address
* We dont need to lookup the cache. */
ptr_ethhdr = net_create_eth_header ((Uint8 *)ptr_iphdr, (void *)&BroadcastMac[0], 0x800);
if (ptr_ethhdr == NULL)
return;
/* We now have a completed Ethernet packet; send it across. */
net_send_packet (ptr_ethhdr, sizeof(ETHHDR) + l3_pkt_size);
/* The packet has been transmitted and we can clean it up now. */
net_free_tx_packet ((Uint8 *)ptr_iphdr);
return;
}
o bootp.c
(C:\ti\pdk_c667x_2_0_5\packages\ti\boot\ibl\src\driver\eth)
- Line 141~149
/* Check if we have exceeded the max. permissible? *
if (bootpmcb.num_request > BOOTP_MAX_RETRIES)
{
/* Error: Maximum retransmissions have been exceeded; indicate error. */
mprintf ("BOOTP Failure: Max Retransmissions exceeded\n");
net_set_error ();
udp_sock_close(bootpmcb.sock);
return;
}
Regards,
j-breeze
Hi Rahul,
My customer solved this issue with their own efforts and told me their tentative workaround as follows(highlighted in red). So, I'd like to close this thread.
I appreciated your support so much.
o icmp.c
(C:\ti\pdk_c667x_2_0_5\packages\ti\boot\ibl\src\driver\eth)
- Line 77~82
//#ifdef BIGENDIAN
if( tmp1 )
TSum += (Uint32)(*pw & 0xFF00);
//#else
// if( tmp1 )
// TSum += (Uint32)(*pw & 0x00FF);
//#endif
o udp.c
(C:\ti\pdk_c667x_2_0_5\packages\ti\boot\ibl\src\driver\eth)
- Line 96~102
//#ifdef BIGENDIAN
if( tmp1 )
TSum += (Uint32)(*pw & 0xFF00);
//#else
// if( tmp1 )
// TSum += (Uint32)(*pw & 0x00FF);
//#endif
Regards,
j-breeze
J-breeze,
Thank you for posting the update here and your patience when working through this issue. I am glad the issue is resolved.
I can confirm that this a bug due to inconsistent BIGENDIAN Macro definition. The C6000 Compiler defines this macro as _BIG_ENDIAN so that macro is incorrectly defined in the IBL code.I will report the bug and ask the development team to fix the bug. If you want the code to work in both little and big endian mode, you can replace BIGENDIAN with _BIG_ENDIAN.
Regards,
Rahul