This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMS320DM8148: 2GB DDR performance issue

Part Number: TMS320DM8148

Tool/software: Linux

Here i am using DM8148 in 8 channel DVR.

DM8148 stat CPU 720Mhz DDR 400Mhz

Previously we are using 1GB DDR and with we getting good performance, but now we had increase the ram to 2GB and we are not getting the performance similar to 1GB, My most of the cpu is used in system.

please find the below data and suggest the memory map require to improve the performance?

  1. With 1GB DDR

-          performance is as below:-

user  

nice

system

idle

iowait

irq

softirq

25.98%

0.00%

47.64%

21.50%

4.28%

0.04%

0.55%

 

-          The memory map as follow:-

linux memory 384MB from 0x80000000 and 256MB from 0xA8000000

 

-          Result of cat /proc/meminfo:-

MemTotal:

621332 kB

MemFree:

69800 kB

Buffers:

2784 kB

Cached:

448836 kB

SwapCached:

0 kB

Active:

214604 kB

Inactive:

265804 kB

Active(anon):

35784 kB

Inactive(anon):

86236 kB

Active(file):

178820 kB

Inactive(file):

179568 kB

Unevictable:

0 kB

Mlocked:

0 kB

HighTotal:

183296 kB

HighFree:

1796 kB

LowTotal:

438036 kB

LowFree:

68004 kB

SwapTotal:

0 kB

SwapFree:

0 kB

Dirty:

8488 kB

Writeback:

0 kB

AnonPages:

28804 kB

Mapped:

89776 kB

Shmem:

93232 kB

Slab:

55244 kB

SReclaimable:

47920 kB

SUnreclaim:

7324 kB

KernelStack:

1520 kB

PageTables:

1576 kB

NFS_Unstable:

0 kB

Bounce:

0 kB

WritebackTmp:

0 kB

CommitLimit:

310664 kB

Committed_AS:

910572 kB

VmallocTotal:

196608 kB

VmallocUsed:

144520 kB

VmallocChunk:

34812 kB

 

  1. With 2GB DDR:-

-          performance is as below:-

 

user  

nice

system

idle

iowait

irq

softirq

27.99%

0.00%

58.50%

6.57%

4.14%

0.01%

2.79%

 

 

 

-          The memory map as below:-

linux memory 384MB from 0x80000000 and 800MB from 0xC0000000

 

-          Result of cat /proc/meminfo:-

 

MemTotal:

1174016kB

MemFree:

951620kB

Buffers:

7992kB

Cached:

156064kB

SwapCached:

0kB

Active:

59724kB

Inactive:

133460kB

Active(anon):

47736kB

Inactive(anon):

91268kB

Active(file):

11988kB

Inactive(file):

42192kB

Unevictable:

0kB

Mlocked:

0kB

HighTotal:

797696kB

HighFree:

603884kB

LowTotal:

376320kB

LowFree:

347736kB

SwapTotal:

0kB

SwapFree:

0kB

Dirty:

28kB

Writeback:

0kB

AnonPages:

29144kB

Mapped:

98400kB

Shmem:

109876kB

Slab:

11516kB

SReclaimable:

5096kB

SUnreclaim:

6420kB

KernelStack:

1688kB

PageTables:

1732kB

NFS_Unstable:

0kB

Bounce:

0kB

WritebackTmp:

0kB

CommitLimit:

587008kB

Committed_AS:

1032000kB

VmallocTotal:

516096kB

VmallocUsed:

144448kB

VmallocChunk:

350744kB