HI everybody ,
please on a AM5728 running Linux , idea is to save some variables/status ( few bystes about 128Bytes in total ) and then force from the command line a reboot ( so SW reboot , no power off ) ( this is due to enter some special configurations/settings etc ) . AM5728 will reset and boot . Due to bug i862 and our workaround all SW resets go to PORZ : are DATA in internal RAM kept or internal RAM Is reinizialided ? any workaround to reboot keeping 1 KBof DATA ?
we can use internal RAM or DDR ( using self refresh for example ) , but what we need on system level is to be able when booting to "see" these variables .
any suggestion @ system level ?
thank you
bye
Carlo