Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3354, OMAPL138
Tool/software: Linux
Hello All,
I am using TI processor AM3354 for development.Where application based on QT with SQLite to store the data.but when compile and try to run QT based SQlite application on target AM335x starter kit then fails and through the error SQL driver are missing.so finally trying to building Processor SDK(processor-sdk-03.02.00.05) and individual components from source using Yocto .But getting the following error:
Cloning into '/home/administrator/tisdk/sources/meta-arago'...
error: Could not resolve host: arago-project.org (curl_result = 6, http_code = 0, sha1 = 4b41ddf38da0b5c6a0458609a36411ed1884336d)
error: Unable to find 700424cdbf608b989615b3b2ff960093fed9e9a9 under arago-project.org/.../meta-arago.git
Cannot obtain needed tree 700424cdbf608b989615b3b2ff960093fed9e9a9
while processing commit d2594fff3e0c5567a26e853de95035337fca52cf.
error: Fetch failed.
The following procedure followed for the building of SDK:
http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK
Thanks,
Anil