This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5505: Multiplexed Pins and GPIO

Part Number: TMS320C5505

I would like to confirm the following issue:

Is it possible to use unused multiplexed pin as GPIO?

For example, 

Set "MMC1, I2S1, and GP[11:6]" pin multiplexing as "MODE 1,." but I want to use "MMC1_D0/I2S1_DX/GP[8]" as GP[8].

(I do not want to use I2S1_DX except I2S1_CLK, I2S1_FS, I2S1_RX.)