Part Number: AM5716
Hello,
I'd like to understand L4 Interconnect. This is because the internal throughput is important for our application.
I think that the following two connections can access simultaneously. (case 1)
- Accessing from MPU to UART1 through the L4_PER1_P3.
- Accessing from EDMA_TC0 to UART7 through the L4_PER2_P1.
How about this case? Can they also access simultaneously? (case 2)
- Accessing from MPU to UART1 through the L4_PER1_P3.
- Accessing from EDMA_TC0 to UART2 through the L4_PER1_P1.
Could you please reply me with Yes or No? Also, if there is a related description in TRM, please let me know.
I'm referring to these figures in TRM(SPRUHZ7E).
- Figure 14-3. Connectivity Matrix
- Figure 14-9. L4 Interconnect Overview
Please see attached the file.
Regards,
Kazu