Dear support,
I am trying to get Ethernet working on a TDA2 SoC with a DP83848Q PHY. I
have reuesed the Ethernet driver from
the VISION_SDK_02_08_00_00; I think this driver should run on the Vayu
board.
On my board I got receive and transmit working with this driver, but I
have noticed that there are packets lost on both
directions (receice and transmit).
On my board only D0 and D1 is connected for transmit and receive to the
DP83848Q. The connection is direct with a 22Ohms series
resistor and not with a multiplexer in between as on the Vayu board. For
the TDA2 SoC I have reused the pad configuration
from the SDK.
I have verified the 50MHz clock for the DP83848Q and TDA2
(RMII0_MHZ_50_CLK) is fine, the reset and power supply of
DP83848Q is stable. Do you have any idea what I could try or what could
cause the packet loss on my setup?
For testing I would like to try to set the PHY to loopback mode; How do we have to setup the GMACSW_Config structure to enable the loopback mode in PHY?
Best regards,
Erwin