This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSDSK6713
Greetings everybody!
I am Akshay. I am trying to use the boards that are avail be in the DSP lab. These are the ones from 2005. The DSP boards number I am trying to connect is TMDSDSK6713. As the lab hasn't been used for a while i don't have access to any of the prerequisite files. If somebody can help me with that it would great. I am using Matlab 2015a and CCSv5.1.1 does board work on these platforms or do I have to use the older versions.?
I am using Matlab 2015a and CCSv5.1.1 does board work on these platforms or do I have to use the older versions.?
Yordan:
Thank you for your response. I am also looking for the basic test program Sine8_LED and the related files like the .lib files, .cmd files, .asm files etc etc.
Thnak you
Akshay
Hey Rahul!
First of thanks for the URL's. I hope they help me. Secondly, The lab I was talking to was organizational specific. Also, if you coulld provide me a set of basic files to run the on the board it would be great.
Thank you.