Part Number: TMS320C6747
Hi,
My customer is using C6747.
They have the same question as E2E below.
e2e.ti.com/.../305054
Is it OK after RESETOUT is released for access to SPI Flash by RBL?
Best Regards,
Miyashiro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6747
Hi,
My customer is using C6747.
They have the same question as E2E below.
e2e.ti.com/.../305054
Is it OK after RESETOUT is released for access to SPI Flash by RBL?
Best Regards,
Miyashiro
Miyashiro-san,
I was unable to find in the documentation where it states that SPI0_SCS[0] or SPI1_SCS[0] will remain high until RESETOUT is deasserted (goes high), but the datasheet does say that "all pins are tri-stated with the exception of RESETOUT which remains active through the reset sequence". See 6.4.1 Power-On Reset (POR).
Therefore, the bootloader cannot possibly attempt to access any memory device until after the pins are released from tri-state (after RESETOUT is released).
RESETOUT will be asserted until the device has completed executing its reset sequence. Table 6-1 in the datasheet specifies 6169 OSCIN cycles, which is between 206uS to 514uS given that OSCIN can be between 12MHz and 30MHz.
Can you just measure the time between RESETOUT and SPI0_SCS[0] or SPI1_SCS[0] going low to verify this?
Hope this helps,
Mark