Tool/software: Linux
Hello,
I'm using J6 Vayu EVM board, I'm looking for support for FQTSS implementation.
As per AVB standard, for implementing FQTSS on end-station (Talker node), Traffic shaper algorithm (Credit-based shaper) should be implemented using hardware packet queue.
When I referred the TRM of J6, it is mentioned as GMAC_SW subsystem supports Audio/Video Bridging (P802.1Qav/D6.0). So I assumed that the board has the capability to implement FQTSS, and so Qav is implemented in CPSW driver.
When I looked the other thread of TI forum for configuring the CPSW driver in kernel, I couldn't get any info. And to my surprise I found few response(which is dated more than a year back) like CPSW driver is not supporting Qav.
I want to know whether in the latest updated CPSW driver supports FQTSS or not. If yes how to configure the same.
Note : I'm using GLSDK 7.04.00.03 and HW is J6 Vayu EVM Rev H.
Regards,
Karikalan