This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi,
TI,
Now I want to build the gstreamer1.0-plugins-ducati of sdk03.01 because of the memory leak of ducatih264enc Gstreamer plugin.
I folllow the steps of below link:
When I build the sdk04.00,it is ok!
./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.00.00.04-config.txt
MACHINE=am57xx-evm bitbake gstreamer1.0-plugins-ducati
But when I build the sdk03.01 like that:
./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-03.01.00.06-config.txt
MACHINE=am57xx-evm bitbake gstreamer1.0-plugins-ducati
It shows me that:
Are there any solution?
BR,
vefone
Hi,
Ramprasad,
I modify sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils-linaro-2.25.inc like that:
releases.linaro.org/.../binutils-linaro-${BPV}-${RELEASE}.tar.xz \ to
releases.linaro.org/.../binutils-linaro-${BPV}-${RELEASE}.tar.xz \
It is ok!
But now there are another error :
ERROR: linux-processor-sdk-4.4.19+gitAUTOINC+db0b54cdad-r7e do_create_srcipk: Function failed: do_create_srcipk (log file is located at /home/vefone/am5728/git-store/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-processor-sdk/4.4.19+gitAUTOINC+db0b54cdad-r7e/temp/log.do_create_srcipk.55502)
ERROR: Logfile of failure stored in: /home/vefone/am5728/git-store/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-processor-sdk/4.4.19+gitAUTOINC+db0b54cdad-r7e/temp/log.do_create_srcipk.55502
Log data follows:
| DEBUG: Executing python function sstate_task_prefunc
| DEBUG: Python function sstate_task_prefunc finished
| DEBUG: Executing shell function do_create_srcipk
| Cloning into '/home/vefone/am5728/git-store/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-processor-sdk/4.4.19+gitAUTOINC+db0b54cdad-r7e/temp-git-shallow-clone'...
| warning: Could not find remote branch processor-sdk-linux-03.01.00 to clone.
| fatal: Remote branch processor-sdk-linux-03.01.00 not found in upstream origin
| fatal: The remote end hung up unexpectedly
| WARNING: /home/vefone/am5728/git-store/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-processor-sdk/4.4.19+gitAUTOINC+db0b54cdad-r7e/temp/run.do_create_srcipk.55502:1 exit 128 from 'git clone --depth 400 --branch processor-sdk-linux-03.01.00 file://$PWD/.git $gitshallowclone'
| ERROR: Function failed: do_create_srcipk (log file is located at /home/vefone/am5728/git-store/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/linux-processor-sdk/4.4.19+gitAUTOINC+db0b54cdad-r7e/temp/log.do_create_srcipk.55502)
ERROR: Task 842 (/home/vefone/am5728/git-store/tisdk/sources/meta-processor-sdk/recipes-kernel/linux/linux-processor-sdk_4.4.bb, do_create_srcipk) failed with exit code '1'
It shows me that there are not processor-sdk-linux-03.01.00 branch at git://git.ti.com/processor-sdk/processor-sdk-linux.git
Any suggestion?
BR,
vefone