Part Number: TMS320C6678
Hi,
My customer is trying to use C6678 SRIO IBIS-AMI model, but they encountered the following error with ADS.
It seems *.dll files has been placed on the same directory with IBIS files, but still they saw erros.
Can you suggest ?
I`m not sure if the related document is existing in IBIS package, but if you have separately, send me, please.
Error detected by hpeesofsim in Tx_AMI1 during netlist flattening.
Unable to load AMI library
'C:\ti\Keystone2\Keystone_SRIO_AIF_Hyperlink_SerDes_AMI_Model_v0p96_r1p2\tx_ibis_ami\librincewind_40nm_tx.dll'.
Please check in your IBIS file whether AMI library (DLL)
for the 32-bit Windows platform is specified and
whether it is stored in the same folder as the IBIS file.
Environment:
- windows7 64bit ADS ver 2016.01.1 (64bit) or
- windows7 64bit ADS 2014.01(64bit) or
- windows7 32bit ADS 2014.01(32bit)
Best Regards,
Naoki Kawada