This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6474EVM Timer interrupt and DSP/Bios



 Hi,

I am using CCS 3.3 version for EVM6474. Also my application uses DSP/Bios kernel in CORE 0. Since my application needs 200 Micro Seconds resolution, I am going for another hardware Timer (lets say Timer 2).

 The Timer interrupt is dispatched with HWI_dispatchPlug() API. In Timer Isr, SEM_postBinary() is called to Trigger a Task which will wait for the Semaphore.

Here the problem starts-> I am getting the Timer interrupt for fixed amount of times only (254 times), also the Task which is waiting for this SEM is getting wake up every 200us (254 times only).  After that CORE 0 gets Restarted.

Can u please help me on this Issue.?

Below is my sample code,

VOID DataIf_TimerIsr(VOID)
{
 DataIf *pThis = &oDataIf;

  SEM_postBinary (&SEM_200us);
 
 nCount++;

 LOG_printf(&trace, " Timer ISR: %d", nCount);

}

VOID DataIf_AssemblerTask(VOID)
{


 DataIf *pThis = &oDataIf;
  while(1)
 {
  SEM_pendBinary (&SEM_200us, SYS_FOREVER);
  LOG_printf(&trace, "Task :%d", nCount);

}

     

Thanks,

Bala

  • My suspicion is that something is causing a stack overflow or stack corruption. Nothing jumps out at me, but there is a lot of other code that you need to examine and debug.

    Curiously, what do you want to really do every 200us? This is obviously sanity-test code, which is certainly a smart thing to do.

    Three things you might try are:

    1. Remove the LOG_printf's or use a counter to only print them once every 50-100 iterations. That is a lot of data to be dumping out.

    2. Try SEM_pend/SEM_post instead of the binary versions. This is not the likely problem, but it might lead to different results that could help you figure out what is wrong.

    3. Turn on optimization to improve the performance of these two functions.

    Please let us know what you find out.

  • Hi Randy,

    Thanks for the suggestions :-)

    I have tried Your suggestions below,

    1. Removing LOG_printf --> no effect

    2. Replacing Binary version of SEM with SEM_pend and SEM_post --> no effect

    3. Turning on Optimization --> Improved the performance but not fully solved (crash occurs below 1ms).

    But,

    After Disabling the PRD module(i.e. Unchecked the PRD module from using the CLK Manager) IT IS WORKING good on even 5 Microseconds.

    Can u please provide comments( Reason) on this.?  

     

    Thanks,

    Bala

  • We can see if anyone in the BIOS forum can help to answer this. The problem would seem to either be a performance issue or a resource conflict issue, at least from what I can picture. The mechanisms for the PRD module and the effect of turning it off will be better understood by the people supporting this BIOS forum.

    If it is a performance issue, then I would have expected removing the 2 LOG_printf statements to have at least increased the number of interrupts before the crash occured, but there was no effect. Yet optimization did have an effect, which again points to a performance issue. So this is confusing for me.

  • I would use the kernel/object view tool and check your stack usage on your tasks.    Adding PRD adds a second interrupt to the system.   Worst case task stack size needs to be able to accomodate 2 HWI interrupt contexts.   ISR itself and nested ISRs along with SWI functions execute on system ISR stack, but the task stack needs to be able to handle 2 HWI contexts.

    So, in your working system, (w/o PRD) it would be good to review your stack usage for all tasks and make sure you have some headroom (300-500 bytes free for each task stack).

    -Karl-

  • Hi Karl,

    I have checked each Task stacks through Kernel object view, it has enough free space.

    can u please give any other suggestions?.

     

    Thanks,

    Bala  

  • No great ideas, unfortunately.    A couple more things to try:


    (1)  can you put a breakpoint on your reset vector?   This address should be in the ISTP register.   Since you say your system "restarts", it must be branching here or something is toggling the reset pin.   If you hit this breakpoint, you might be able to look at kernel/object view (KOV) at this point and see something.  B3 should contain function return pointer. (not sure if reset would clear the regsiters,  I think not, but it has been awhile).


    (2)  can you change your interrupt rate to 2ms (instead of 200us)?  200us should work, but it would be useful to know if this makes a difference.

    (3)  can you run all code/data from internal memory?   That device has a bunch of on-chip memory.  would be good to remove external memory and EMIF and cache from the equation.

  • (4) Check the system stack, in addition to the task stacks that you have already checked. Or just increase it by a significant amount, like +50%. You set the system stack size in the DSP/BIOS configuration GUI (open the .tcf file) under System.MEM->Properties - Stack Size (MAUs). BIOS's scheduler and SWIs (like PRD functions) and interrupts use the system stack.

  • Hi Randy,

    I have checked, increasing the Stack size by 50%.

    but, it gives the same Result.

    here is my .cmd file sections, any suggestions on this?,

    SECTIONS
    {
    .far:scratch1 align=256> L1D_RAM
    .far:scratch2 align=256> L1D_RAM

    .boot: > L2RAM
    .text: > C0_DDR_PROG_RAM
    .cio: > C0_DDR_DATA_RAM
    .vectors: > C0_DDR_PROG_RAM
    .fasttext: > C0_DDR_DATA_RAM
    .cinit: > C0_DDR_DATA_RAM
    .bss: > L2RAM
    .const: > C0_DDR_DATA_RAM
    .far: > C0_DDR_DATA_RAM
    .switch: > C0_DDR_DATA_RAM
    .pinit > C0_DDR_DATA_RAM
    .printf > C0_DDR_DATA_RAM

    }

    Also, please find the attached .Tcf file(change the .txt extention to .tcf).

    Thanks

    Bala 

  • Did you try Karl's primary 3 suggestions? Mine was just a fourth to add to that list.

    You seem to have conflicting uses of L1D SRAM. This memory is flexible in that it can be used as SRAM or as Cache, but these uses are in direct conflict with each other in terms of the use of portions of the physical L1D RAM memory range from 0x00f00000 to 0x00f07fff. When you configure any part as cache, that amount of L1D SRAM is reduced from the higher addresses down. L1D SRAM, if any is available, always starts at 0x00f00000.

    If you configure BIOS to have 32K Cache in L1D, then no L1D SRAM space is available. If you manually define an "L1D_RAM" memory component in BIOS and assign variables to use that space, such as .far:scratch1, then you create a memory conflict that will have devastating results.

    BIOS automatically creates an L1D_CACHE memory component for you when you set the cache size in BIOS. This is intended to force you to avoid that memory range in your application by not allowing you to create another memory component in the same address range. It is not a perfect implementation, since it does not follow every change such as changing to 0K Cache, but it is a good implementation.

  • Looks like you are using standard TI EVM board.  If so, we can reproduce here.

    Can you please make a .zip file with all the files necessary to rebuild your sample app -- we need the .pjt and all the .c and .tci, .h, etc files.

    Please be clear on what the failure mode is.  That is, if we put breakpoint on main(), it sounds like we will hit this b/p after 254 (or similar) interrupts meaning that the code has reset/restarted?

    Thanks,
    -Karl-

  • Sorry Karl & Randy, I am not able to get approval for sending the zipped file(Source file) from my Higher management.

    I have checked your suggestions, and here is my observation below link,

    http://e2e.ti.com/support/embedded/f/355/p/65645/240879.aspx#240879

    Can u please give any other suggestions.?

     

     

    Thanks,

    Bala

     

  • In order to avoid having 2 threads going, I am going to mark that other post  "answered" and reference this post.

    Please put additional information here so we can track it in one place.  Multiple posts on same issue make tracking and support all the more difficult.

    I did not see specific answers to my 3 recommendations.

    One other idea (based on the exception on that other post) is that  you are getting an exception.  The NMI return pointer (NRP) points to the instruction at/near the source of the exception.  Can you look at NRP and see if that's a clue?

    We need a test case to reproduce here.  Can you make a test case w/o any proprietary code so we can reproduce?  Without a test case and/or additional information, we can't do much.

    Thanks,
    -Karl-

     

  • Hi Randy and Karl,

    Here i am happy to inform you that the Issue got solved,

    just by increasing the main Stack size and re-organizing the memory.

    Thanks for your valuable responses and suggestions :-).

    Thanks,

    Bala